2021-06-20 4:32 PM
Hi!
This might be a simple question, but I still haven't solved it.
I want to create an external trigger source for SDADC 16-bit and I have selected TIM12 Capture Compare 1 as external trigger source.
Then I have enable the Output Compare, because I did not find Capture Compare.
Then I enable the NVIC for the SDADC.
HAL_TIM_Base_Start(htim13); /* TIM13 is trigger source for SDADC1 */
HAL_TIM_Base_Start(htim12); /* TIM12 is trigger source for SDADC2 */
HAL_TIM_Base_Start(htim16); /* TIM16 is trigger source for SDADC3 */
if (HAL_SDADC_InjectedStart_IT(hsdadc1) != HAL_OK)
Error_Handler();
if (HAL_SDADC_InjectedStart_IT(hsdadc2) != HAL_OK)
Error_Handler();
if (HAL_SDADC_InjectedStart_IT(hsdadc3) != HAL_OK) /* Differential only */
Error_Handler();
But still. Nothing happens when I have this function avaiable.
This never calls. Why?
/* Callbacks for SDADC */
void HAL_SDADC_InjectedConvCpltCallback(SDADC_HandleTypeDef *hsdadc){
if(hsdadc->Instance == SDADC1) {
STM32_PLC_Analog_Input_SDADC1(hsdadc);
}else if (hsdadc->Instance == SDADC2) {
STM32_PLC_Analog_Input_SDADC2(hsdadc);
}else if (hsdadc->Instance == SDADC3) {
STM32_PLC_Analog_Input_SDADC3(hsdadc);
}
}
Solved! Go to Solution.
2021-06-20 5:22 PM
Include your chip part number.
You start the timer, but I don't see you starting the channel anywhere. Should be a call to HAL_TIM_OC_Start or similar.
2021-06-20 5:22 PM
Include your chip part number.
You start the timer, but I don't see you starting the channel anywhere. Should be a call to HAL_TIM_OC_Start or similar.
2021-06-21 3:16 AM
If you want to trigger the SDADC using a signal coming from outside the STM32, you have to set the timer's channel to Input Capture.
Read the timer chapter in RM.
JW
2021-06-21 3:37 AM
So if I want a trigger source that using a signal inside the STM32. How should I do then?
2021-06-21 3:45 AM
Did not work to use HAL_TIM_OC_Start(htim, TIM_CHANNEL_x)
2021-06-21 3:58 AM
By the way!
It's working now!
Mode in CubeMX need to be Toggle On Match.
Code:
static uint32_t Channel = 0;
static uint32_t SDADC_Single[12];
static uint32_t SDADC_Differential[5];
void STM32_PLC_Start_Analog_Input(TIM_HandleTypeDef* htim12, TIM_HandleTypeDef* htim13, TIM_HandleTypeDef* htim16, SDADC_HandleTypeDef* hsdadc1, SDADC_HandleTypeDef* hsdadc2, SDADC_HandleTypeDef* hsdadc3) {
HAL_TIM_OC_Start(htim13, TIM_CHANNEL_1); /* TIM13 is trigger source for SDADC1 */
HAL_TIM_OC_Start(htim12, TIM_CHANNEL_1); /* TIM12 is trigger source for SDADC2 */
HAL_TIM_OC_Start(htim16, TIM_CHANNEL_1); /* TIM16 is trigger source for SDADC3 */
if (HAL_SDADC_InjectedStart_IT(hsdadc1) != HAL_OK)
Error_Handler();
if (HAL_SDADC_InjectedStart_IT(hsdadc2) != HAL_OK)
Error_Handler();
if (HAL_SDADC_InjectedStart_IT(hsdadc3) != HAL_OK) /* Differential only */
Error_Handler();
}
void STM32_PLC_Analog_Input_SDADC1(SDADC_HandleTypeDef* hsdadc1) {
SDADC_Single[Channel] = HAL_SDADC_InjectedGetValue(hsdadc1, &Channel); /* Channel will have the numbers 0,1,2,3,4,5,6,7,8 but randomly */
}
void STM32_PLC_Analog_Input_SDADC2(SDADC_HandleTypeDef* hsdadc2) {
SDADC_Single[Channel + 9] = HAL_SDADC_InjectedGetValue(hsdadc2, &Channel); /* Channel will have the numbers 0,1,2 but randomly */
}
void STM32_PLC_Analog_Input_SDADC3(SDADC_HandleTypeDef* hsdadc3) {
uint32_t value = HAL_SDADC_InjectedGetValue(hsdadc3, &Channel); /* Channel will have the numbers 0,2,4,6,8 but randomly */
switch(Channel) {
case 0:
SDADC_Differential[0] = value;
break;
case 2:
SDADC_Differential[1] = value;
break;
case 4:
SDADC_Differential[2] = value;
break;
case 6:
SDADC_Differential[3] = value;
break;
case 8:
SDADC_Differential[4] = value;
break;
}
}
void STM32_PLC_Analog_Input_SDADC1_Set_Prescaler(TIM_HandleTypeDef* htim13, uint16_t prescaler){
htim13->Instance->PSC = prescaler;
}
void STM32_PLC_Analog_Input_SDADC2_Set_Prescaler(TIM_HandleTypeDef* htim12, uint16_t prescaler){
htim12->Instance->PSC = prescaler;
}
void STM32_PLC_Analog_Input_SDADC3_Set_Prescaler(TIM_HandleTypeDef* htim16, uint16_t prescaler){
htim16->Instance->PSC = prescaler;
}
/* Get ADC0 to ADC11 */
uint16_t STM32_PLC_Analog_Input_GetADC(uint8_t i){
return SDADC_Single[i];
}
/* Get DADC0 to DADC4 */
uint16_t STM32_PLC_Analog_Input_GetDADC(uint8_t i){
return SDADC_Differential[i];
}
/* Callbacks for SDADC */
void HAL_SDADC_InjectedConvCpltCallback(SDADC_HandleTypeDef *hsdadc){
if(hsdadc->Instance == SDADC1) {
STM32_PLC_Analog_Input_SDADC1(hsdadc);
}else if (hsdadc->Instance == SDADC2) {
STM32_PLC_Analog_Input_SDADC2(hsdadc);
}else if (hsdadc->Instance == SDADC3) {
STM32_PLC_Analog_Input_SDADC3(hsdadc);
}
}