cancel
Showing results for 
Search instead for 
Did you mean: 

How can I get voucher code for P-L496G-CELL 02 after accidentally erased the startup FW?

Ccui.1
Associate II

I accidentally overwrote the FW loaded by ST for P-L496G-CELL 02. So I cannot access the voucher code. Is there any way to retrieve the voucher code?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
S.Ma
Principal

I used to play with this kit in the past, and here was the original "restore my kit" binary.

It might not be the latest one. It's here in case it helps.

Connect STLink, use it as USB Memory stick and drag and drop/flash the bin file if the board is up and ready, configured as in the insert card inside pages pictures.

View solution in original post

2 REPLIES 2
S.Ma
Principal

I used to play with this kit in the past, and here was the original "restore my kit" binary.

It might not be the latest one. It's here in case it helps.

Connect STLink, use it as USB Memory stick and drag and drop/flash the bin file if the board is up and ready, configured as in the insert card inside pages pictures.

Ccui.1
Associate II

It works. Thanks.