2018-10-30 02:08 AM
I just purchased the STM3221G-EVAL board and I am working through some examples. I am currently using running the HMAC example and it runs fine. However I am unable to get the HMAC to match the test vectors provided in the specification (https://tools.ietf.org/html/rfc2202).
Specifically for the following:
test_case = 1
key = 0x0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b
key_len = 20
data = "Hi There"
data_len = 8
digest = 0xb617318655057264e28bc0b6fb378c8ef146be00
But I get a completely different digest.
Any ideas?
Many thanks in advance.
2018-10-30 05:44 AM
> Any ideas?
I don't think so, at least not until you show us your code which doesn't work as expected :-)
2018-10-30 06:24 AM
Thanks [After Forever] - that was just a "hello world"
Here is the code:
/**
******************************************************************************
* @file HASH/HASH_HMAC_SHA1MD5/Src/main.c
* @author MCD Application Team
* @brief This example provides a short description of HASH digest calculation
* using SHA1 and MD5 example.
******************************************************************************
* @attention
*
* <h2><center>© COPYRIGHT(c) 2017 STMicroelectronics</center></h2>
*
* Redistribution and use in source and binary forms, with or without modification,
* are permitted provided that the following conditions are met:
* 1. Redistributions of source code must retain the above copyright notice,
* this list of conditions and the following disclaimer.
* 2. Redistributions in binary form must reproduce the above copyright notice,
* this list of conditions and the following disclaimer in the documentation
* and/or other materials provided with the distribution.
* 3. Neither the name of STMicroelectronics nor the names of its contributors
* may be used to endorse or promote products derived from this software
* without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
* IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
* DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT HOLDER OR CONTRIBUTORS BE LIABLE
* FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL
* DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
* SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER
* CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
* OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
******************************************************************************
*/
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/** @addtogroup STM32F2xx_HAL_Examples
* @{
*/
/** @addtogroup HMAC_SHA1_MD5
* @{
*/
/* Private macro -------------------------------------------------------------*/
/* Private variables ---------------------------------------------------------*/
/* HASH handler declaration */
HASH_HandleTypeDef HashHandle;
/*
"The hash processor is a fully compliant implementation of the secure
hash algorithm (SHA-1), the MD5 (message-digest algorithm 5) hash
algorithm and the HMAC (keyed-hash message authentication code)
algorithm suitable for a variety of applications.*** STM32 ***"
*/
#define cINPUT_TAB_SIZE ((uint32_t) 8)/* The size of the input data "cInput" */
#define cKEY_TAB_SIZE ((uint32_t) 20)
// hex for "Hi There"
__ALIGN_BEGIN const uint8_t cInput[cINPUT_TAB_SIZE] __ALIGN_END = {0x48, 0x69, 0x20, 0x54, 0x68, 0x65, 0x72, 0x65};
__ALIGN_BEGIN const uint8_t cKey[cKEY_TAB_SIZE] __ALIGN_END = {,
0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b,
0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0xb0,
0xb0, 0xb0, 0xb0, 0x0b};
__ALIGN_BEGIN static uint8_t cSHA1Digest[20] __ALIGN_END;
__ALIGN_BEGIN static uint8_t cExpectSHA1Digest[20] __ALIGN_END = {0xb6, 0x17, 0x31, 0x86, 0x55, 0x05, 0x72, 0x64,
0xe2, 0x8b, 0xc0, 0xb6, 0xfb, 0x37, 0x8c, 0x8e,
0xf1, 0x46, 0xbe, 0x00};
/* Private function prototypes -----------------------------------------------*/
static void SystemClock_Config(void);
static void Error_Handler(void);
/* Private functions ---------------------------------------------------------*/
/**
* @brief Main program
* @param None
* @retval None
*/
int main(void)
{
/* STM32F2xx HAL library initialization:
- Configure the Flash prefetch, instruction and Data caches
- Configure the Systick to generate an interrupt each 1 msec
- Set NVIC Group Priority to 4
- Global MSP (MCU Support Package) initialization
*/
HAL_Init();
/* Configure the system clock to 120 MHz */
SystemClock_Config();
/* Configure LED1, LED3 and LED4 */
BSP_LED_Init(LED1);
BSP_LED_Init(LED3);
BSP_LED_Init(LED4);
/****************************************************************************/
/*************************** HMAC-SHA1 2 ************************************/
/****************************************************************************/
BSP_LED_Off(LED1);
HAL_HASH_DeInit(&HashHandle);
HashHandle.Init.DataType = HASH_DATATYPE_8B;
HashHandle.Init.pKey = (uint8_t*)cKey;
HashHandle.Init.KeySize = cKEY_TAB_SIZE;
if(HAL_HASH_Init(&HashHandle) != HAL_OK)
{
Error_Handler();
}
/* Compute HMAC-SHA1 */
if(HAL_HMAC_SHA1_Start(&HashHandle, (uint8_t*)cInput, cINPUT_TAB_SIZE, cSHA1Digest, 0xFF) != HAL_OK)
{
Error_Handler();
}
/* Compare computed digest with expected one */
if(memcmp(cSHA1Digest, cExpectSHA1Digest, sizeof(cExpectSHA1Digest)/sizeof(cExpectSHA1Digest[0])) != 0)
{
Error_Handler();
}
else
{
BSP_LED_On(LED1);
}
/****************************************************************************/
/*************************** HMAC-SHA1 2 repeat *****************************/
/****************************************************************************/
BSP_LED_Off(LED1);
HAL_HASH_DeInit(&HashHandle);
HashHandle.Init.DataType = HASH_DATATYPE_8B;
HashHandle.Init.pKey = (uint8_t*)cKey;
HashHandle.Init.KeySize = cKEY_TAB_SIZE;
if(HAL_HASH_Init(&HashHandle) != HAL_OK)
{
Error_Handler();
}
/* Compute HMAC-SHA1 */
if(HAL_HMAC_SHA1_Start(&HashHandle, (uint8_t*)cInput, cINPUT_TAB_SIZE, cSHA1Digest, 0xFF) != HAL_OK)
{
Error_Handler();
}
/* Compare computed digest with expected one */
if(memcmp(cSHA1Digest, cExpectSHA1Digest, sizeof(cExpectSHA1Digest)/sizeof(cExpectSHA1Digest[0])) != 0)
{
Error_Handler();
}
else
{
BSP_LED_On(LED1);
}
}
/**
* @brief System Clock Configuration
* The system Clock is configured as follow :
* System Clock source = PLL (HSE)
* SYSCLK(Hz) = 120000000
* HCLK(Hz) = 120000000
* AHB Prescaler = 1
* APB1 Prescaler = 4
* APB2 Prescaler = 2
* HSE Frequency(Hz) = 25000000
* PLL_M = 25
* PLL_N = 240
* PLL_P = 2
* PLL_Q = 5
* VDD(V) = 3.3
* Flash Latency(WS) = 3
* @param None
* @retval None
*/
static void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
/* Enable HSE Oscillator and activate PLL with HSE as source */
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 25;
RCC_OscInitStruct.PLL.PLLN = 240;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 5;
if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
clocks dividers */
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief This function is executed in case of error occurrence.
* @param None
* @retval None
*/
static void Error_Handler(void)
{
/* Turn LED3 on */
BSP_LED_On(LED3);
while(1)
{
}
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
/**
* @}
*/
/**
* @}
*/
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
2018-10-30 06:37 AM
Now compare the key you mentioned and the key you wrote:
0x0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b0b
0x0b0b0b0b0b0b0b0b0b0b0b0b0b0b0bb0b0b0b00b
2018-10-30 06:56 AM
Aha - thanks.
Fixed it but still no match.
__ALIGN_BEGIN const uint8_t cInput[cINPUT_TAB_SIZE] __ALIGN_END = {0x48, 0x69, 0x20, 0x54, 0x68, 0x65, 0x72, 0x65};
__ALIGN_BEGIN const uint8_t cKey[cKEY_TAB_SIZE] __ALIGN_END = {0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b,
0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b, 0x0b,
0x0b, 0x0b, 0x0b, 0x0b};
2018-10-30 07:01 AM
Here is what I get:
0x75733ACAE127DD1DBFB2F8156E6A6E0C650B94B2