2018-11-03 01:41 PM
2018-11-03 01:41 PM
Does Suresh have a question?
2018-11-03 01:45 PM
yes. I cant use my stlink and blue pill module, STM32F103C8 (Blue PILL) and STM32F103CB6T(STLINK clone). Driver not properly not installed and also I cant debug and flash my target board.
I got below error
Target not found,
2018-11-03 01:49 PM
Target core not powered.
SWDIO/SWCLK not correctly connected.
ST-LINK not connected to VTarget and GND.
2018-11-03 01:51 PM
3.3 to 3.3
gnd to gnd
swio to io
clk to clk
2018-11-03 01:52 PM
this is forum also looking great like arduino
2018-11-03 01:53 PM
thanks for buddy for replying
2018-11-03 01:53 PM
in india the time is 2:23 AM
2018-11-03 05:29 PM
And you've measured 3 or 3.3V ?
I'm not using blue pill boards, if it has a USB port you could try pulling the BOOT0 pin high and seeing if will connect in DFU mode. If so you could use the Cube STM32 Programmer application.