cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, Kindly help me in solving this issue.

jennifer_dsilva
Associate II
 
9 REPLIES 9
Ozone
Lead II

Being more descriptive with your issue, already at the headline, would help a lot.

The STM32 discovery boards use to have ST-Link debug adapters, not OpenOCD.

Or do you have replaced the ST-Link firmware on your board ?

turboscrew
Senior III

Looks like you are using wrong setup files for openOCD. Which debug interface are you using?

At least SWD should work fine with OpenOCD - I've been using the Eclipse-OpenOCD-ST-link-mini for quite a while.

There could also be ST-link USB-driver missing.

What's your board? Are you using ST-link-v2? Or maybe an on-board debug HW?

No..I did not replaced the st-link

jennifer_dsilva
Associate II

I am also using the same. Eclipse-OpenOCD

Hello,

Thanks for the reply .

my settings are

board : STM32F407VGTX DISCOVERY BOARD (old)

I downloaded the latest AC6 system workbench from openstm32.org

i also installed stlink drivers from here https://www.st.com/en/development-tools/stsw-link009.html

and interestingly it works on other PC but having issue on mine.

I dont understand what is missing in my PC ?

Brian Kling
Senior III

@jennifer_dsilva​ you created this post 3 times, so I deleted the other two posts. Please only post a question once; otherwise it is a mess if people start responding in several places, thanks!

Also as mentioned, when you post a question, please describe:

  1. What the issue is, what product(s) are you using and what are you trying to accomplish
  2. What you have tried, with what results
  3. What do you need

Can't you configure your project to use the ST-Link debugger instead ?

Would be the easiest way.

> ... you created this post 3 times, so I deleted the other two posts. Please only post a question once; otherwise it is a mess if people start responding in several places, thanks!

I use to blame the awkward and un-intuitive forum software.

Not that it hadn't been mentioned, but there are nice and stable forum platforms available. (Just check some competitiors ... :o )

Why has ST to come up with something extraordinary each time ?

turboscrew
Senior III

Maybe your OpenOCD configuration file is wrong?

In debugger tab (don't remember by heart) there should be something like "-f boards/stm32f4discovery.cfg"