2023-01-24 4:09 AM
2023-01-24 4:57 AM
Welcome, @Nicolò Meloncelli, to the community!
This has nothing to do directly with the STM32CubeIDE, but with the character set that your display supports. You would have to look at its datasheet and find out if it has the DEGC character in its character set. If it does, you would have to send its hex code as a character, but that would only apply to that particular display.
Does it answer your question?
Regards
/Peter
2023-01-24 7:00 AM
Hi Peter,
with the following code variation I've the symbol "°" in the display. I don't know why I can't write == '°' and leave "°C" instead of =='?' and " ?C". If I do so the if condition is skipped.
2023-01-24 10:46 AM
Well, you have not yet inserted the character set of your two-line LCD here. As a rule, the character set only partially matches that in operating systems such as Windows, Linux or MacOS, mostly only in the ASCII range 0x20 (space)...0x7D (left curly bracket).
However, on many of these LCDs, the question mark is usually coded with 0x3F and the degree sign with 0xDF.
You should now check:
I would also check how the display routine converts the bytes to be sent to the LCD from the input string.
By the way: please be so kind and do not post source code snippets as screenshots, but for better readability and testability with the code snippet button </> below the text box.
Regards
/Peter
2023-01-24 11:01 AM