Hi, do any of you know how to achieve the advertised MHz ADC sampling rates on the Arduino H7 Portenta board, which I believe has STM32 H7?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-07-27 3:41 AM
I tried the STM32Cube Programmer but it could not connect to the board. I'm on Linux Manjaro. Many thanks
- Labels:
-
ADC
-
STM32H7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-07-28 3:31 AM
Thank you Tesla,
just to clarify, I am trying to connect to the board via USB cable.
Parity even doesn't make a difference and I struggle with finding out how to set BOOT0 on the Portenta H7 board. I came across this post:
including a comment by TDK:
"Looks like the USB connector on that board is using the HS USB which is not supported by the STM32 bootloader."
to which reefwing replied:
"The Portenta can do both HS and FS USB however Arduino devices have a proprietary USB VID/PID"
Do the errors I get make sense in this context? Any idea how to connect to the board using FS USB?
However, returning to my initial question, my goal is to achieve the advertised ADC rates for this particular board. In the meantime, I have found a promising tutorial at https://deepbluembedded.com/stm32-adc-read-example-dma-interrupt-polling/ which uses the STM32CubeMX to generate some background code. Most of the hal libraries have been ported by the arduino people, so my next approach would be to generate the setup code (main.h and Init functions) for the STM32H747XI (thank you @reefwing !) and incorporating that using the arduino IDE.
If this approach works, I will not need to use the STM32CubeProgrammer to connect to the board. I'll post any progress here.
Many thanks for your help!

- « Previous
-
- 1
- 2
- Next »