cancel
Showing results for 
Search instead for 
Did you mean: 

Help to identify the component

Mtrev
Visitor

I need to know if this ST i'm using has been made by ST or is a clone

 

G071GB

GQ28L10

9RCHNB

.       323


1 ACCEPTED SOLUTION

Accepted Solutions

9R is TSMC Fab 14 in Taiwan, for STMicro

Pull the PCN from Digikey's STM32G071GB page

https://mm.digikey.com/Volume0/opasdata/d220001/medias/docus/6346/Microcontrollers-24-14864.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

5 REPLIES 5
AScha.3
Chief III

Why you think, its a clone ?

+

What telling CubeProgrammer , after connect ? (show...)

If you feel a post has answered your question, please click "Accept as Solution".

9R is TSMC Fab 14 in Taiwan, for STMicro

Pull the PCN from Digikey's STM32G071GB page

https://mm.digikey.com/Volume0/opasdata/d220001/medias/docus/6346/Microcontrollers-24-14864.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

This STM has strange functioning after an update, this STM is connected on an Eletronic speed controller and not working after updates.

I've attached an printscreen of programmer.

You'd need to work with the vendor more directly to understand if this is the correct firmware, applied appropriately.

You could dump/inspect the FLASH via STM32 Cube Programmer, making sure it's got the binary data, and hasn't written the .HEX as ASCII into the device.

I don't see anything from your presentation so far that the part is not legitimate, but you'd need to check the circuit / PCB to confirm you're working with the right firmware.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
STOne-32
ST Employee

Dear @Mtrev ,

It can be a change in our bootloader version creating this change at your application level , please check the bootloader version ID between old devices and this new ones check updates in AN2606 and also the version of the devices .  Let us know 

Ciao

STone-32