2023-05-11 5:34 AM
Hello everyone :D
I am currently using the STM32H743VIT6 (LQFP-100) on a custom PCB.
My goal is to generate fast positive pulses (ideal case would be a 10ns pulse) on TIM4 CH2 (PB8). APB2 is clocked at 200MHz so I can get 5ns ticks from my timer.
Generating 100ns wide pulses is quite easy using PWM by placing "Pulse" parameter on 16bits to 19 = (20-1) since 100ns/5ns = 20.
Problem is: if I want to narrow this pulse to 50ns for example, the trace of the signal starts to become rounded and doesn't reach 3.3V on top.
I suspect it is because of the rise/fall times which are about 30ns each.
Second problem is: When I change OSPEEDR register to VERY_HIGH, the rise/fall times are only reduced by a few nanoseconds while the datasheet shows rise/fall times less than 5ns for my range of capacitive load and supply (3.3V). I have estimated the capacitive load to be approx. 40pF.
Can someone enlighten me please ? :folded_hands:
2sayle
Solved! Go to Solution.
2023-05-12 12:43 AM
Thank you all for your answers. Indeed, I am not used to probing on PCBs. Your advice has been invaluable! Do you have any manuals/tutorials that I can use to improve my hardware testing skills?
2023-05-12 2:16 AM
there are some good white papers and app notes , look at Ti, Analog Devices, Tektronix...
https://e2e.ti.com/blogs_/#pifragment-322110PostSortBy=MostComments
https://www.ti.com/lit/an/slyt627/slyt627.pdf
2023-05-12 2:35 AM
Thank you !