2012-12-10 1:37 PM
hello forum ,
I am trying to run a TCP/IP demo on a Olimex STM32F4 board
with eclipse + yagarto
however I cannot connect to the board with LAN
when I stop the demo with JTAG to look where it hangs
it shows below code
I tried to set up breakpoint before the memcpy function
as shown in the attached picture
It stops at the breakpoint just before the memcpy function
however when I rerun from this point
it ends up at hardfault handler as shown below
please advice how can I proceed ?
void
HardFault_Handler(
void
)
{
/* Go to infinite loop when Hard Fault exception occurs */
while
(1){
}
}
2012-12-18 1:36 PM
2012-12-18 2:08 PM
Are you sure it doesn't fault because it leaves main()? Where does it go then?
Try putting a while(1); at the end so it stays within main()2012-12-19 1:26 AM
hello
of course I have memcpy inside infinite loop I omitted it for simplicity of the message the micro still goes into hardfault when it sees memcpy how much simpler can a memcpy command be ( previous post ) ? I suspect that the linkerscript is somehow bad can you please comment on my linkerscript ? thanks2012-12-19 2:19 AM
Is it possible that you link to a wrong library ?
If the library code contains ARM32 instructions, it will surely hardfault. Make sure you link to a THUMB/THUMB2 library.2012-12-19 4:26 AM
If in doubt disassemble the code. I don't think the linker script is the issue.
2012-12-19 1:58 PM
2012-12-19 3:48 PM
The ''blx 0x800B584'' is indicative of a call to 32-bit ARM code, you could look at 0x800B584 to confirm this. This would suggest your linker is pulling in 32-bit libraries (ARM7/ARM9) instead of the 16-bit Thumb libraries.
The 16-bit memcpy should look a bit like this, from my .LSS listing file08000188 <
memcpy
>:
8000188: 2a0f cmp r2, #15
800018a: b4f0 push {r4, r5, r6, r7}
800018c: d940 bls.n 8000210 <
memcpy
+0x88>
800018e: ea41 0300 orr.w r3, r1, r0
8000192: 079b lsls r3, r3, #30
8000194: d13e bne.n 8000214 <
memcpy
+0x8c>
8000196: 460c mov r4, r1
8000198: 4603 mov r3, r0
800019a: 4615 mov r5, r2
800019c: 6826 ldr r6, [r4, #0]
800019e: 3d10 subs r5, #16
80001a0: 601e str r6, [r3, #0]
80001a2: 6866 ldr r6, [r4, #4]
80001a4: 605e str r6, [r3, #4]
80001a6: 68a6 ldr r6, [r4, #8]
A typical compiler command line
arm-none-eabi-gcc -c -mcpu=cortex-m3 -mthumb -O3 -ffunction-sections -fdata-sections -Wall -Wstrict-prototypes -Wextra -std=gnu89 -g -ggdb3 -fverbose-asm -Wa,-ahlms=out/usbd_msc_bot.lst -DUSE_STDPERIPH_DRIVER -DSTM32F4XX -DUSE_STM32F4_DISCOVERY -DUSE_USB_OTG_FS -DHSE_VALUE=8000000 -MD -MP -MF out/usbd_msc_bot.d -I. -Iinc usbd_msc_bot.c -o out/usbd_msc_bot.o
A typical linker command line
arm-none-eabi-g++ -mcpu=cortex-m3 -mthumb -Tstm32f4xx.ld -g -Wl,-Map=out/demo.map,--cref,--no-warn-mismatch -Wl,--gc-sections -nostartfiles out/startup_stm32f4xx.o out/app.o out/misc.o out/stm32f4_discovery.o out/stm32f4_discovery_sdio_sd.o out/stm32f4xx_dma.o out/stm32f4xx_gpio.o out/stm32f4xx_rcc.o out/stm32f4xx_sdio.o out/stm32fxxx_it.o out/system_stm32f4xx.o out/usb_bsp.o out/usb_core.o out/usb_dcd.o out/usb_dcd_int.o out/usbd_core.o out/usbd_desc.o out/usbd_ioreq.o out/usbd_msc_bot.o out/usbd_msc_core.o out/usbd_msc_data.o out/usbd_msc_scsi.o out/usbd_req.o out/usbd_storage_msd.o out/usbd_usr.o out/test.o -o out/demo.elf
2012-12-22 9:35 AM
Hello Clive ,
you are really a great person I added below switches to linker command line and the program linked succesfully with correct library before : LDFLAGS=
-g -v -nostartfilesnow : LDFLAGS
= -
mcpu
=cortex-m3 -mthumb -g -v -nostartfiles and the TCP / IP demo run succesfully - I can connect to my Olimex STM32-E407 board through LAN thank you and other who replied to my post