2019-01-26 12:13 PM
Actually I did not purchase one yet. I know I have to choose one with a bootloader CAN include like a STM32F412.
Is there a GUI who allow a drag & drop to flash the board, using CAN ?
I saw that STM32CubeProgrammer should be update to allow to flash the board using bootloader CAN but I don't know when.
If you have any other advice, it will be appreciated.
Regards,
Zephyr
2019-01-26 12:56 PM
The Cube programmer offers CAN as a Mode for the ST-LINK connectivity.
As the creator of a CAN product why would you not have the ability to build both ends of the connection to implement your own tools?
2019-01-28 2:00 AM
Hello Clive,
First, thanks for your answer.
My goal is to save time. Why couldn't I use fonctions that are implemented by ST ? like the bootloader and their soft ? They're here for that.
Then, I don't understand. If I use the CAN mode with a ST-LINK V3, I could flash my board through bootloader CAN using the "start programming" button, couldn't I ?