cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I would like to update my board firmware using bootloader CAN. Could the STLINK-V3 allow me to flash my board using bootloader CAN ? otherwise, which kind of board should I use as a host PC ?

Zephyr S
Associate II

Actually I did not purchase one yet. I know I have to choose one with a bootloader CAN include like a STM32F412.

Is there a GUI who allow a drag & drop to flash the board, using CAN ?

I saw that STM32CubeProgrammer should be update to allow to flash the board using bootloader CAN but I don't know when.

If you have any other advice, it will be appreciated.

Regards,

Zephyr

2 REPLIES 2

The Cube programmer offers CAN as a Mode for the ST-LINK connectivity.

As the creator of a CAN product why would you not have the ability to build both ends of the connection to implement your own tools?

0690X000006DFcWQAW.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Zephyr S
Associate II

Hello Clive,

First, thanks for your answer.

My goal is to save time. Why couldn't I use fonctions that are implemented by ST ? like the bootloader and their soft ? They're here for that.

Then, I don't understand. If I use the CAN mode with a ST-LINK V3, I could flash my board through bootloader CAN using the "start programming" button, couldn't I ?