2021-02-08 8:26 AM
2021-02-10 6:19 AM
Apart from setting HDSEL bit, there is no much difference to full-duplex UART. Just keep in mind that the RX will always be active and TX will "take over" the pin when data is transmitted. RX will even receive the same data that TX is transmitting. Therefore the code has to ignore it or turn RX off during transmission. And of course the software has to manage concurrency to not try to receive and transmit simultaneously.
2021-02-10 8:05 AM
I find solution!
Initialization:
void MX_USART1_UART_Init(void)
{
LL_USART_InitTypeDef USART_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_USART1);
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_GPIOB);
/**USART1 GPIO Configuration
PB6 ------> USART1_TX
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_6;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_OPENDRAIN;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
LL_GPIO_AF_EnableRemap_USART1();
/* USART1 interrupt Init */
NVIC_SetPriority(USART1_IRQn, NVIC_EncodePriority(NVIC_GetPriorityGrouping(), 15, 0));
NVIC_EnableIRQ(USART1_IRQn);
USART_InitStruct.BaudRate = 115200;
USART_InitStruct.DataWidth = LL_USART_DATAWIDTH_8B;
USART_InitStruct.StopBits = LL_USART_STOPBITS_1;
USART_InitStruct.Parity = LL_USART_PARITY_NONE;
USART_InitStruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
USART_InitStruct.OverSampling = LL_USART_OVERSAMPLING_16;
LL_USART_Init(USART1, &USART_InitStruct);
LL_USART_ConfigHalfDuplexMode(USART1);
LL_USART_Enable(USART1);
LL_USART_EnableHalfDuplex(USART1);
LL_USART_EnableIT_RXNE(USART1);
}
For select rx mode:
LL_USART_DisableDirectionTx(USART1);
LL_USART_EnableDirectionRx(USART1);
For select tx mode:
LL_USART_DisableDirectionRx(USART1);
LL_USART_EnableDirectionTx(USART1);