2023-07-17 5:33 AM
Hello everyone:
I have a problem with my project.
My project is to use STM32H750UBKx + Keil MDK5 IDE to design.
The customer bootloader runs in Flash, and The application runs in Quad SPI NOR Flash (or SRAM).
Problem: When I execute the code "JumpToApplication();", it will be "Hardfault"
Thanks!
more information:
0. I have checked that the data in the SRAM(0x30000000) is the same as the bin content compiled by my application.
1. The fault reporter(debug):
2.My Bootloader code are:
void RunApplication(void)
{
extern volatile uint8_t arrAppBuff[100 * 1024];
MemCpy((uint8_t *)arrAppBuff, (uint8_t *)0x90000000, 100*1024);
uint32_t nAppAddr = 0x30000000;
uint32_t JumpAddress = *(__IO uint32_t*)((nAppAddr) + 4);
pFunction JumpToApplication = (pFunction)JumpAddress;
printf("Jump!\n");
HAL_RCC_DeInit();
HAL_DeInit();
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
SCB->VTOR = (nAppAddr);
__set_PRIMASK(1);
__set_MSP(*(__IO uint32_t*)(nAppAddr));
__set_CONTROL(0);
JumpToApplication();
}
3. Application code:
int main(void)
{
__disable_irq();
SCB->VTOR = 0x30000000;
__enable_irq();
SCB_EnableICache();
SCB_EnableDCache();
HAL_Init();
SystemClock_Config();
PeriphCommonClock_Config();
}
4. Application 's scatter file:
LR_IROM1 0x30000000 0x00048000 { ; load region size_region
ER_IROM1 0x30000000 0x00048000 { ; load address = execution address
*.o (RESET, +First)
*(InRoot$$Sections)
.ANY (+RO)
.ANY (+XO)
}
RW_IRAM_DTCM 0x20000000 0x00020000 { ; 128k
.ANY (+RW +ZI)
;* (.ram.tcm)
* (.DTCMshared, +Last)
}
RW_IRAM_AXI 0x24000000 0x0007C000 { ;512k - 16k = 496k
.ANY (+RW +ZI)
* (.sram123_shared, +Last)
}
RW_IRAM4 0x38000000 0x00010000 { ;64k
.ANY (+RW +ZI)
}
}
Solved! Go to Solution.
2023-07-17 7:28 PM
LOL, The reason is my customer bootloader is use "V6.16 ARM compiler", and the application uses "V5.06 ARM compiler".
Boot compiler:
App compiler:
2023-07-17 7:09 PM
Looks like jump to 0 (corrupted pointers or variables on stack?). Try to debug, single step from your bootloader to few first instructions of the app reset handler.
2023-07-17 7:28 PM
LOL, The reason is my customer bootloader is use "V6.16 ARM compiler", and the application uses "V5.06 ARM compiler".
Boot compiler:
App compiler:
2023-07-19 4:09 PM
Compiler version is not the cause the issue. Your broken code is!