Hard - to catch - fault
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 12:50 AM
Hello,
I have a kind of strange issue. When I really stress my system (it handles serial packets, get the right data, and send it via serial, I send thousands of messages without waiting for reply), in an unpredictable way, I sometimes get an invalid PC load usage fault of invalid state fault. When I get an invalid PC load usage, the program counter is like 0x0 or 0x5, or sometimes it contains a ram address, but I don't have code in ram, and looking at the stack trace, I have the feeling there is a stack pointer corruption somewhere because some of the registers have flash address of branch code in them (and LR has weird stuff, obviously not flash code nor ram address). Here are my stack traces :****************************
HARD FAULT !Stack = 0x20000660
Invalid PC load usage fault at Program counter = 0x200082B0Stack frame :
R0 = 0x400264B8 R1 = 0x20008318 R2 = 0x3C R3 = 0x200082B0 R12 = 0x0 LR = 0x8002417 PC = 0x200082B0 PSR = 0x20008318****************************
Or :
****************************
HARD FAULT !Stack = 0x20000688
Invalid state usage fault at Program counter = 0x20008270Stack frame :
R0 = 0x20008288 R1 = 0x20008EA8 R2 = 0x3C R3 = 0x200082B0 R12 = 0x0 LR = 0x20008270 PC = 0x20008270 PSR = 0x20000200****************************
Or again:
****************************
HARD FAULT !Stack = 0x20000670
Invalid PC load usage fault at Program counter = 0x1Stack frame :
R0 = 0x0 R1 = 0x80023D7 R2 = 0x8003B26 R3 = 0x21000200 R12 = 0x0 LR = 0x8003279 PC = 0x1 PSR = 0x200082B0****************************
The problem seems to happen (tried to track it down but it's very hard) on the service call interrupt exit after a malloc call (but there is like 10000 malloc calls without problem first). My process stacks are far from full (half empty at min), I have 8k of system stack. The hard fault happens with user stack, but again, seems to trigger when popping rgisters at service call exit. Spent about 10 hours trying to fix this, but no luck so far, do youguys have any advice for me? Thomas. #dma2- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 1:27 AM
[Update #1]
If I don't actually send the data through serial, no hard fault, I do prepare the buffer for DMA, etc, but don't trigger the DMA send, and I can ''handle'' hundreds of thousands of messages. As soon as I really enable the transmit DMA, I can get hard faults anytime. The DMAtriggers an interrupt when it ends, but even if the ISR is empty, I have hard faults (in normal condition when the DMA ends the ISR checks if there is more data to send, prepare a buffer and re-trigger a DMA). I'm already using DMA for serial reception, with ISRs, etc, and this seems to work flawlessly. I have 2 levels of interrupt pre-emption, highest is for service call and systick, the other for ISRs and PendSV (which has lowest priority):NVIC_SetPriorityGrouping(6); // there is only 2 levels of preemption, one for system, the other for interrupts. This gives 8 levels of sub-priority for interrupts.
NVIC_SetPriority(SVCall_IRQn, 0x00); // set service call priority to highest and preemptive
NVIC_SetPriority(SysTick_IRQn, 0x7F); // set systick interrupt to low but preemptive
NVIC_SetPriority(PendSV_IRQn, 0xFF); // set pend sv interrupt to low and not preemptive
Thomas.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 1:41 AM
[Update #2]
If I do disable the TX DMA interrupt, but still send data (using the DMA CR bit 0 to know if DMA has ended, and I can send a new buffer), then I still have hard faults. So far it seems the transmit DMA itself is the root cause of my problems :( Thomas.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 2:01 AM
Tried to lower the speed of the MCU to 40MHz ... I now have :
****************************
HARD FAULT !Stack = 0x20000688
Imprecise data bus error.Stack frame :
R0 = 0x100F241 R1 = 0x100F240 R2 = 0x1 R3 = 0x20008190 R12 = 0x0 LR = 0x80018BF PC = 0x80018E8 PSR = 0x1000200****************************
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 2:08 AM
Had the imprecise error only once ...
****************************
HARD FAULT !Stack = 0x20000678
Invalid PC load usage fault at Program counter = 0x0Stack frame :
R0 = 0x20008190 R1 = 0x2000A078 R2 = 0x20008130 R3 = 0x2000A078 R12 = 0x3C LR = 0x20008190 PC = 0x0 PSR = 0x80031B3****************************
****************************
HARD FAULT !Stack = 0x20000688
Invalid state usage fault at Program counter = 0x20008128Stack frame :
R0 = 0x20008140 R1 = 0x20009440 R2 = 0x3C R3 = 0x20008168 R12 = 0x0 LR = 0x20008128 PC = 0x20008128 PSR = 0x20000200****************************
****************************
HARD FAULT !Stack = 0x20000688
Invalid state usage fault at Program counter = 0x20008128Stack frame :
R0 = 0x20008168 R1 = 0x200081A8 R2 = 0x3C R3 = 0x20008190 R12 = 0x0 LR = 0x20008128 PC = 0x20008128 PSR = 0x20000200****************************
****************************
HARD FAULT !Stack = 0x20000660
Invalid PC load usage fault at Program counter = 0x20008168Stack frame :
R0 = 0x1 R1 = 0x20009270 R2 = 0x3C R3 = 0x20008168 R12 = 0x0 LR = 0x8002413 PC = 0x20008168 PSR = 0x20009270****************************
****************************
HARD FAULT !Stack = 0x20000688
Invalid state usage fault at Program counter = 0x20008128Stack frame :
R0 = 0x20008140 R1 = 0x20009440 R2 = 0x3C R3 = 0x20008168 R12 = 0x0 LR = 0x20008128 PC = 0x20008128 PSR = 0x20000200****************************
****************************
HARD FAULT !Stack = 0x20000680
Invalid PC load usage fault at Program counter = 0x4Stack frame :
R0 = 0x20008140 R1 = 0x1 R2 = 0x0 R3 = 0x800103B R12 = 0x8003B22 LR = 0x81000000 PC = 0x4 PSR = 0x20003658****************************
****************************
HARD FAULT !Stack = 0x20000678
Invalid PC load usage fault at Program counter = 0x800328BStack frame :
R0 = 0x8003B22 R1 = 0x21000200 R2 = 0x20008140 R3 = 0x8003275 R12 = 0x1 LR = 0x20009740 PC = 0x800328B PSR = 0x800106B****************************
****************************
HARD FAULT !Stack = 0x20000678
Invalid PC load usage fault at Program counter = 0x0Stack frame :
R0 = 0x20008168 R1 = 0x20009450 R2 = 0x20008158 R3 = 0x20009450 R12 = 0x3C LR = 0x20008168 PC = 0x0 PSR = 0x80031B3****************************
****************************
HARD FAULT !Stack = 0x20000688
Invalid state usage fault at Program counter = 0x20008168Stack frame :
R0 = 0x20008118 R1 = 0x2000A080 R2 = 0x3C R3 = 0x20008150 R12 = 0x0 LR = 0x20008168 PC = 0x20008168 PSR = 0x20000200****************************
****************************
HARD FAULT !Stack = 0x20000660
Invalid PC load usage fault at Program counter = 0x20008168Stack frame :
R0 = 0x2000A070 R1 = 0x2000A070 R2 = 0x3C R3 = 0x20008168 R12 = 0x0 LR = 0x8002423 PC = 0x20008168 PSR = 0x2000A070****************************
****************************
HARD FAULT !Stack = 0x20000680
Invalid PC load usage fault at Program counter = 0x7Stack frame :
R0 = 0x20008118 R1 = 0x1 R2 = 0x0 R3 = 0x800103B R12 = 0x8003B22 LR = 0x81000000 PC = 0x7 PSR = 0x20003658****************************
****************************
HARD FAULT !Stack = 0x200006A8
Invalid PC load usage fault at Program counter = 0x0Stack frame :
R0 = 0x80018A1 R1 = 0x20008140 R2 = 0x0 R3 = 0x0 R12 = 0x0 LR = 0x0 PC = 0x0 PSR = 0x8002A1B****************************
****************************
HARD FAULT !Stack = 0x20000660
Invalid PC load usage fault at Program counter = 0x20008168Stack frame :
R0 = 0x2000A070 R1 = 0x2000A070 R2 = 0x3C R3 = 0x20008168 R12 = 0x0 LR = 0x8002423 PC = 0x20008168 PSR = 0x2000A070****************************
It seems to hard fault much faster at 40MHz speed than 120MHz. Thomas.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 2:16 AM
Post the code where you fill the DMA registers.
JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 2:56 AM
Hello,
Here it is :DMA2_Stream7->CR = 0x8000450; // configures DMA to memory to peripheral byte transfer
DMA2_Stream7->PAR = (uint32_t) (&(USART1->DR)); // peripheral register is USART1 data register
DMA2_Stream7->FCR = 5; // use FIFO with half full trigger.
Then when I triger transmit :
DMA2_Stream7->M0AR = (uint32_t)_transmitBuffer;
DMA2_Stream7 ->NDTR = count;
DMA2_Stream7 ->CR |= 1; // enable DMA.
Just saw anytime the transmit DMA end interrupt triggers, I have the FIFO error bit set ... I wasn't using the FIFO so I enabled it with half empty trigger (FCR = 5), nothing changed.
Thomas.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 3:12 AM
Seems that with debugger not attached, the hard fault doesn't trigger (about 1M packets replied without it stopping) ...
Thomas.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 3:25 AM
Wow.
What debugger/IDE do you use? Did you have extensive number of breakpoints set? Did you have some ''live'' data/register displayed? JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-04 3:25 AM
Tried with ST Link (was using J-Link FLASHER ARM), same result, hard fault with debuger attached, no hard fault when debugger not attached (as the stack is corrupted, I wouldn't expect it to recover, plus I have a while(1) loop at the end of hard fault handler ISR).
Thomas.