HAL_UART_Transmit_IT only send first letter
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-21 1:31 AM
I am very new to use hal_usartTransmit_it because I use only usart_transmit() , which is the blocking mode.
I changed all of my transmit() code to transmit_it() for better performance, but after that my ble send message only shows buffer's first letter
Could you give some advice?
my usart init code
huart2.Instance = USART2;
huart2.Init.BaudRate = 9600;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
HAL_NVIC_EnableIRQ(USART2_IRQn);
HAL_NVIC_SetPriority(USART2_IRQn, 1, 0);
__HAL_UART_ENABLE_IT(&huart2 , UART_IT_RXNE ); //uart rx it ON
in Main
txBuffer = "ABCDEF";
txSize=6
if(HAL_UART_Transmit_IT(&huart2 , (uint8_t*)txBuffer , txSize)!= HAL_OK)
{
Error_Handler();
}
but I only receive 'A'.
my Usart Interrupt Handler, mainly for the receive_it handling.
*/
void USART2_IRQHandler(void)
{
HAL_NVIC_DisableIRQ(USART2_IRQn);
HAL_NVIC_DisableIRQ(DMA1_Channel1_IRQn);
usart_intCount++;
uint8_t tempBuffer[20]={0,};
HAL_UART_IRQHandler(&huart2);
HAL_UART_Receive(&huart2,tempBuffer,20, 0 );
int i=0;
while(tempBuffer[i] ){
if(tempBuffer[i]>47 && tempBuffer[i]<58 ){ //숫�??
buffer[bufferIndex] = tempBuffer[i];
bufferIndex+=1;
}
else if(tempBuffer[i] >64 && tempBuffer[i] < 91){ //대문�??
buffer[bufferIndex] = tempBuffer[i];
bufferIndex+=1;
}
i++;
}
for(int i=0;i<bufferIndex;i++){
if(buffer[i] == 'F'){ //F RECEIVED? -> anyway, read the buffer !
needCallback=1;
bufferIndex=0;
break;
}
} //reading tempBuffer and move to -> buffer
rxReady=1;
HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
HAL_NVIC_EnableIRQ(USART2_IRQn);
}
Thanks for reading.
- Labels:
-
UART-USART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-10-21 1:44 AM
I won't go through all details of our code. If you are using HAL, use a completion callback too:
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
...
}and don't fiddle in the USART2_IRQHandler directly. Especially don't call a blocking function (HAL_UART_Receive) in the IRQ handler.
The basic flow is
char ch;
main:
HAL_UART_Receive_IT( &huart2, &ch, 1 );
HAL_UART_RxCpltCallback:
// process ch (global variable)
// re-enable interrupt handling for receiving next char
HAL_UART_Receive_IT( &huart2, &ch, 1 );There are more advanced solutions see https://stm32f4-discovery.net/2017/07/stm32-tutorial-efficiently-receive-uart-data-using-dma/