2015-02-12 2:51 AM
Hi, I'm having a problem that when calling HAL_UART_TRANSMIT_DMA() I require a delay between consecutive calls of the function for it to accept new data into the DMA. I've found adding a HAL_Delay between calls fixes the problem so I must be trying to call the transmit too often.
How do I go about creating a while(dma_busy_flag){} for the DMA here? I'm using these settings:stm32f4xx_hal_msp.c (some code not shown) extern DMA_HandleTypeDef hdma_usart1_tx; hdma_usart1_tx.Instance = DMA2_Stream7; hdma_usart1_tx.Init.Channel = DMA_CHANNEL_4; hdma_usart1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_usart1_tx.Init.PeriphInc = DMA_PINC_DISABLE; hdma_usart1_tx.Init.MemInc = DMA_MINC_ENABLE; hdma_usart1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE; hdma_usart1_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE; hdma_usart1_tx.Init.Mode = DMA_NORMAL; hdma_usart1_tx.Init.Priority = DMA_PRIORITY_LOW; hdma_usart1_tx.Init.FIFOMode = DMA_FIFOMODE_DISABLE; hdma_usart1_tx.Init.MemBurst = DMA_MBURST_SINGLE; hdma_usart1_tx.Init.PeriphBurst = DMA_PBURST_SINGLE; HAL_DMA_Init(&hdma_usart1_tx); __HAL_LINKDMA(huart, hdmatx, hdma_usart1_tx); stm32f4xx_it.c (some code not shown) void DMA2_Stream7_IRQHandler(void) { HAL_NVIC_ClearPendingIRQ(DMA2_Stream7_IRQn); HAL_DMA_IRQHandler(&hdma_usart1_tx); }serial.c (some code not shown) HAL_NVIC_SetPriority(DMA2_Stream7_IRQn, 5, 0); HAL_NVIC_EnableIRQ(DMA2_Stream7_IRQn); /* Prints the supplied string to uart */ void print(char string[]) { // Do we need a ''while(dma_busy){}''? HAL_UART_Transmit_DMA(&huart1, (uint8_t*)string, strlen(string)); } /* UART TX complete callback */ void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart) { // Do we need a ''clear_dma_busy_flag''? }I've tried using the macros:__HAL_DMA_GET_FLAG(&hdma_usart1_tx, DMA_FLAG_TCIF3_7)__HAL_DMA_CLEAR_FLAG(&hdma_usart1_tx, DMA_FLAG_TCIF3_7)but haven't had any luck. Is there somewhere I'm messing up?(Also unrelated, how do i format posts on this forum for code?) #brought-to-you-by-microsoft(tm) #i-can''t-help-you-with-that2015-02-12 6:51 AM
I've managed to get a bit further by using
while(HAL_UART_Transmit_DMA(....) != HAL_OK) {}in my print function. The problem is that now after a few transfers, the function gets stuck as not_ok and sits in the loop forever.my problem could simply be that im calling transmit too often and i could just join strings together before sending them out. Though I don't want to use this as a work around if I'm not using the DMA in a robust manner.If I use HAL_UART_Transmit_IT, the same thing happens. The UART transmit seems to get stuck because ''HAL_UART_STATE_BUSY_RX_TX''.2015-02-12 8:58 AM
With the SPL we either spin on the DMA TC, or chain the next string at the DMA TC interrupt.
The HAL adds a level of awkwardness I'm not willing to buy into.2015-02-12 9:00 AM
(Also unrelated, how do i format posts on this forum for code?)
It's that obvious ''Paintbrush [<>]'' icon with the ''Format Code Block'' hover tip, in the top left of the Word-in-a-Box(tm) interface.