cancel
Showing results for 
Search instead for 
Did you mean: 

HAL driver I2C with stm32F0 - init and transmit

uli
Associate II
Posted on February 13, 2015 at 09:28

 

 

The original post was too long to process during our migration. Please click on the attachment to read the original post.
1 REPLY 1
Amel NASRI
ST Employee
Posted on February 16, 2015 at 13:16

Hello,

I don't see in your code where exactly is enabled the I2C clock?

Check your project & try to call it after GPIO initilaization.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.