cancel
Showing results for 
Search instead for 
Did you mean: 

USB FIle download ->''Snow'' on LCD

Johanan1
Associate II
Posted on February 14, 2015 at 16:33

Using USB and FATFS, I am downloading a large file from USB to external flash (approx 2 MB), during download, I can see small random ''snow'' white pixels on LCD screen.

The file download is a separate FreeRTOS task, with no GUI interface whatsoever.

What could be the problem? do I need to make some synchronization between USB activity and LCD controller? (It could be due to bus issue as the frame buffer and flash are external memories)

Johanan
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
AvaTar
Lead
Posted on February 16, 2015 at 13:22

I'd guess either power issues (with supply voltage drops), or interrupt load issues, if you clock the display directly from a MCU peripheral.