2017-05-09 1:28 PM
hi
this code which i use >> (shift operator) to detect flag work correctly
void putchar( char *string)
{ while(*string) { while(usart_sr >> 6 == RESET); while(usart_sr >> 7 == RESET); USART_SendData(USART2,*string); *string++; }}but when i change it from & and some value of hex, the does not work correctly
void putchar( char *string)
{ while(*string) { while(usart_sr & 0x80 == RESET); while(usart_sr & 0x40 == RESET); USART_SendData(USART2,*string); *string++; }}is there someone to explain why?
thanks
#flagselect ##operators2017-05-09 3:01 PM
The bit shift doesn't do what you think it does, and you should also use brackets to be more explicit about ordering
while((USART2->SR & 0x80) == RESET);
I don't know where you get usart_sr from but USART2->SR is volatile so the compiler will always re-read it regardless of optimization level.
2017-05-09 9:55 PM
Also, assuming usart_sr is some byte value and bits 6 or 7 are set, in the first example you are shifting them to the LSB and seeing if it's equal to RESET which presumably equals 1
In the second example, firstly you have reversed the order in which the bits are tested. 0x80 is the seventh bit and 0x40 is the 6th. Secondly if these bits are set you will end up with values 0x80 and 0x40 in each statement which, judging from example 1, cant equal RESET.
If you want to wait while bit 7 is set
while(usart_sr & 0x80);
If you want to wait while bit 7 is clear
while(!(usart_sr & 0x80));
2017-05-09 11:40 PM
Sorry,Ä° have forgotten to mention what is usart_sr .
Usart_sr is just uint32_t pointer to SR register of usart2
2017-05-10 9:09 AM
RESET in this case will be zero.
The SR is at least 16-bit wide, shifting it does not extract singular bits.
If usart_sr is a pointer you'd presumably want to use *usart_sr to read the content of the pointer rather than act on the value of the pointer itself (ie the address)