Strange operation of Nx_WebServer example on STM32H735G-DK board
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-06-03 2:31 PM
I am experimenting with the function of reading a file by receiving a user command in the Nx_WebServer example of STM32H735G-DK.
When connecting Stlink, input the t key in the Com port (115200 bps) that appears and press Enter to read the dashboard.html file.
After performing this function, a fault occurs in tx_event_flags_get(&finish_flag, 0x01, TX_AND_CLEAR, &actual_flags, TX_WAIT_FOREVER); of console.c that is executed.
This event flag is for communication between the UART receive interrupt and console_thread, and it works normally if filex io is not performed.
Please help me figure out why this problem occurs after calling the filex API.
Labels:
- Labels:
-
STM32H7 Series
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-06-04 8:03 PM
Hello
after increasing stack size of console thread into 4K, the problem disappeared.
Thanks