2010-06-01 01:38 AM
Graphic Library firmware
#unavailable-resources #unavailable-resources #setting-a-bad-example #stm322011-05-17 04:53 AM
For the benefit of other forum members here's a link to the document referred to.
2011-05-17 04:53 AM
If the library was on ST's site it'd expect it to be here
http://www.st.com/stonline/products/support/micro/files/an3128.zip Since it isn't either it isn't posted yet (the AN is only a few weeks old) or its somewhere else. Where did you find the original link to AN3128? Its not on the main STM32 download page at http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=1102011-05-17 04:53 AM
I don't remember , probably I find the document on
http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&fam=110
but now is not here.I'll wait for the zip file. Regards. Stefano2011-05-17 04:53 AM
Any news regarding source code described by
AN3128
.Luminary
Micro provide free graphics libraries. What are the plans ofSTMicroelectronics
? Regards,2011-05-17 04:53 AM
Maybe it's another one that you have to specifically request?
See:
[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/AN2799 - STM32 and STPM01 - Source Code&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/AN2799 - STM32 and STPM01 - Source Code&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E2011-05-17 04:53 AM
Hi All,
I went on a ST seminar in Rousset (France).
They said that this graphics library will be available during 1st quarter of 2011.
You have to wait.
Philippe
2011-05-17 04:53 AM
Dear All,
We are pleased to inform you that the STM32 Embedded GUI library release is now available(attached). Please refer to application note AN3128 for a complete description of the graphical library Objects/API.
The full package contains the STM32 Embedded GUI library and demonstrations firmware as well as a software application Resource Editor (User Interface).
2011-05-17 04:53 AM
Great step from STM.
Thanks a lot.2011-05-17 04:53 AM
Hi,
Is the Firmware supports working with foreign languages fonts? work with unicode? if yes how?