GPIO - arduino pin mapping for STM32F769I-discovery?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-23 9:35 PM
Hi , I have succesfuly managed to merge the GPIO example code into my project.
I am using the audio application project as the base project.
The GPIO button toggles the LED.
I would like to define 3 GPIO pins as digital ouputs on the arduino headers of the STM32F769I-discovery board
so far I have code below, but can't find the arduino pin : GPIO pin map ?
can arduino pins GPIO ? or should I be doing this a different way ? I just need to toggle 3 pins high and low.
static void EXTI0_GPIO_BEN(void)
{ GPIO_InitTypeDef GPIO_InitStructure;/* Enable GPIOC clock */
__HAL_RCC_GPIOA_CLK_ENABLE();// configure gpio pins for reset for external adc dsp and dac devices
// gpio reset for ADC
GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Pull = GPIO_NOPULL; // no pullup or pull dowm resistors ? GPIO_InitStructure.Pin = GPIO_PIN_0; // gpio reset for DSP GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Pull = GPIO_NOPULL; // no pullup or pull dowm resistors ? GPIO_InitStructure.Pin = GPIO_PIN_1; // gpio reset for DAC GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStructure.Pull = GPIO_NOPULL; // no pullup or pull dowm resistors ? GPIO_InitStructure.Pin = GPIO_PIN_1;HAL_GPIO_Init(GPIOA, &GPIO_InitStructure); /// go initilize pins ?
// i don't think I need to have interrupts for this ??
/* Enable and set EXTI line 0 Interrupt to the lowest priority */
// HAL_NVIC_SetPriority(EXTI0_IRQn, 2, 0); // HAL_NVIC_EnableIRQ(EXTI0_IRQn);}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 1:50 AM
so far I have code below, but can't find the arduino pin : GPIO pin map ?
UM2033 Table 13 and Fig.33
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 4:43 AM
,
,
Hi waclawek,
I looked at table 13 but cannot see how it relates to GPIO pin definition in example GPIO code.
for example which physical pin in table 13 is GPIO_PIN_0 , ?
GPIO_InitStructure.Pin = GPIO_PIN_0,
from the table,
pin number , , , , , , pin name , , , , , label , , , , , , , , , , , , , , , , , , , , , comment
C2 , , , , , , , , , , , , , , , , , , , , PI8 , , , , , , , , , , , GPIO_Input , , , , , , , , , NC4
from GPIO example,
/** @defgroup GPIO_pins_define GPIO pins define
,
, * @{,
, */,
♯ define GPIO_PIN_0 , , , , , , , , , , , , , , , , ((uint16_t)0x0001U) , /* Pin 0 selected , , , */,
♯ define GPIO_PIN_1 , , , , , , , , , , , , , , , , ((uint16_t)0x0002U) , /* Pin 1 selected , , , */,
♯ define GPIO_PIN_2 , , , , , , , , , , , , , , , , ((uint16_t)0x0004U) , /* Pin 2 selected , , , */,
♯ define GPIO_PIN_3 , , , , , , , , , , , , , , , , ((uint16_t)0x0008U) , /* Pin 3 selected , , , */,
♯ define GPIO_PIN_4 , , , , , , , , , , , , , , , , ((uint16_t)0x0010U) , /* Pin 4 selected , , , */,
♯ define GPIO_PIN_5 , , , , , , , , , , , , , , , , ((uint16_t)0x0020U) , /* Pin 5 selected , , , */,
♯ define GPIO_PIN_6 , , , , , , , , , , , , , , , , ((uint16_t)0x0040U) , /* Pin 6 selected , , , */,
♯ define GPIO_PIN_7 , , , , , , , , , , , , , , , , ((uint16_t)0x0080U) , /* Pin 7 selected , , , */,
♯ define GPIO_PIN_8 , , , , , , , , , , , , , , , , ((uint16_t)0x0100U) , /* Pin 8 selected , , , */,
♯ define GPIO_PIN_9 , , , , , , , , , , , , , , , , ((uint16_t)0x0200U) , /* Pin 9 selected , , , */,
♯ define GPIO_PIN_10 , , , , , , , , , , , , , , , ((uint16_t)0x0400U) , /* Pin 10 selected , , */,
♯ define GPIO_PIN_11 , , , , , , , , , , , , , , , ((uint16_t)0x0800U) , /* Pin 11 selected , , */,
♯ define GPIO_PIN_12 , , , , , , , , , , , , , , , ((uint16_t)0x1000U) , /* Pin 12 selected , , */,
♯ define GPIO_PIN_13 , , , , , , , , , , , , , , , ((uint16_t)0x2000U) , /* Pin 13 selected , , */,
♯ define GPIO_PIN_14 , , , , , , , , , , , , , , , ((uint16_t)0x4000U) , /* Pin 14 selected , , */,
♯ define GPIO_PIN_15 , , , , , , , , , , , , , , , ((uint16_t)0x8000U) , /* Pin 15 selected , , */,
♯ define GPIO_PIN_All , , , , , , , , , , , , , , ((uint16_t)0xFFFFU) , /* All pins selected */♯ define GPIO_PIN_MASK , , , , , , , , , , , , , ((uint32_t)0x0000FFFFU) /* PIN mask for assert test */
,
/**,
, * @},
, */- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 5:38 AM
In Tab13, search for lines where in Comment the name starts with ARD_. Fig.33 may be more comprehensive.
I am not going comment on the example code and 'libraries'.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 5:53 AM
Your code in your first post shows how to initialize a gpio pin.
The relevant files are stm32f7xx_hal_gpio.h and stm32f7xx_hal_gpio.c
Its just a connector on a board. there is no arduino gpio api in the HAL.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 6:29 AM
Thanks Waclawek , helpful
still don't know how to define a GPIO pin though. I should have guessed ARD was Arduino !
Maybe it would help if I knew the hardware address of say ARD_D0 ? Then I could work backwards
through the libraries / code to see the relationship.
Anyone know where I can find that information ?
does GPIO_PIN_0 or hardware address 0x0001 = ARD_D0 ?
maybe i'm looking for the hardware address of ARD_D0 , ARD_D1 etc
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 7:59 AM
I'd maybe forget about looking for and usingthe BSP defines, you have the info you need on the schematic
ARD_D0 is shown as PC7
To use that as an output you have to enable the GPIO clock for GPIO C and init the pin(s) as so:
GPIO_InitTypeDef GPIO_InitStructure;
__HAL_RCC_GPIOC_CLK_ENABLE();
GPIO_InitStructure.Pin = GPIO_PIN_6 | GPIO_PIN_7 | GPIO_PIN_8;
GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_OD; //GPIO_MODE_OUTPUT_PP; // ;GPIO_MODE_OUTPUT_OD
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStructure.Pull = GPIO_NOPULL; // GPIO_PULLDOWN;
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
(I've also defined PC6 and PC8 as outputs above)
If you wanted to use the pins as part of a peripheral like I2C / SPI then you need to look at the examplesin the _msp files. These are where the GPIO is configuredvia callback from the HAL eg, within HAL_I2C_Init()
void HAL_I2C_MspInit(I2C_HandleTypeDef *hi2c)
{
GPIO_InitTypeDef GPIO_InitStruct;
.
.
/* Enable DMAx clock */
I2Cx_DMA_CLK_ENABLE();
/*##-3- Configure peripheral GPIO ##########################################*/
/* I2C TX GPIO pin configuration */
GPIO_InitStruct.Pin = I2Cx_SCL_PIN;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = I2Cx_SCL_SDA_AF;
HAL_GPIO_Init(I2Cx_SCL_GPIO_PORT, &GPIO_InitStruct);
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?.
.
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
In this case, the I/O is #defined in a Board Support header file somewhere... when writing your own projects, I would recommend putting all the I/O setup in one place and replacing the #defines with actual pin numbers so you can see what's going on a bit easier.
egI2Cx_SCL_PIN might be GPIO_PIN_8 andI2Cx_SCL_GPIO_PORT might be GPIOBfor the processor you're using
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 8:40 AM
Maybe it would help if I knew the hardware address of say ARD_D0 ? Then I could work backwards through the libraries / code to see the relationship.
Anyone know where I can find that information ?
does GPIO_PIN_0 or hardware address 0x0001 = ARD_D0 ?
maybe i'm looking for the hardware address of ARD_D0 , ARD_D1 etc
'ARD_D0' is just an arbitrary name for a signal/connection in the schematics.
Down to the right of your image, at CN13, you see an instance of ARD_D0, and directly to the left, 'PC7'.
This PC7 is the actual GPIO pin of the MCU used to provide that 'ARD_D0' functionality.
You will find the pin name PC7 in the usual documents (as Jan suggested).
With time and experience, you gonna get use to read schematics.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 9:27 AM
thank for this, so I can use these as digital output if I initialise them as such ?
PC02 = GPIO_PIN_2 = ARD_A2 ( arduino anlouge pin 2 )
PC06 = GPIO_PIN_6 = ARD_D1 ( arduino digital pin 1 )
PC07 = GPIO_PIN_7 = ARD_D0 ( arduino digital pin 0 )
PC08 = GPIO_PIN_8 = ARD_D5 ( arduino digital pin 5 )
are there any other physical GPIO pins available as digital outputs on the STM32F769I-discovery ?
what does PCx , PFx , PAx etc stand for ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-04-24 12:03 PM
I took a look at stm32f7xx_hal_gpio.c and came up with...
HAL_GPIO_WritePin(GPIOA, 7,1); // GPIO_PIN_6 , ARD_D0 HIGH
HAL_Delay(500); HAL_GPIO_WritePin(GPIOA, 7,0); // GPIO_PIN_6 , ARD_D0 LOWHAL_Delay(500);HAL_GPIO_WritePin(GPIOA, 7,1); // GPIO_PIN_6 , ARD_D0 HIGH
HAL_Delay(500);Will try it now and report back here if it works.
I noticed HAL_GPIO_TogglePin() but thought I'd try WritePin first.
I'm not really sure what GPIOA is doing and having a guess 0 is off and 1 is on !