2015-12-09 06:11 AM
Overview
Thehttps://github.com/gnuarmeclipse
includes a set of open source Eclipse plug-ins and tools to create/build/debug/manageARM
(32-bits) andAArch64
(64-bits) applications and static/shared libraries, using the latestGNU ARM GCC
toolchains.Eclipse Marketplace
Aiming to further improve the user experience while installing/updating the plug-ins, theGNU ARM Eclipse
project was registered tohttps://marketplace.eclipse.org/content/gnu-arm-eclipse
:Benefits
The main advantage of using the Eclipse Marketplace is asimplified install procedure
, no longer requiring to manually enter the update site address.The Install button
The Eclipse Marketplace not only provides a centralised index to locate projects, it goes one step further and provides a drag-and-drop browser button.drag-and-drop the button to a running Eclipse
, and the plug-ins to install/update will be automatically identified:More info
For more details about theGNU ARM Eclipse
project, please refer to the project site .