cancel
Showing results for 
Search instead for 
Did you mean: 

Glass LCD STM32L0

bhavesh
Associate II
Posted on April 13, 2016 at 23:25

Hi,

I facing problem with custom segment glass LCD interfacing which include 4 COM pin and 20 SEGMENT pin with 1/4 duty cycle and 1/3 bias (Refer Attachment).

I tries to understanding HAL library provided on ST site example project but, I can't understand the RAM part.

Please suggest me, is more information/documents require to interface Glass LCD ? 

Please help me.

thank you.

#glass-lcd #stm32l0
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Abhishek Gupta
Associate III

Do you find any solution regarding this custom glass.\

If yes Than please share me the some solution so that i also can drive it.