cancel
Showing results for 
Search instead for 
Did you mean: 

Getting started .

LalalandAudio
Associate II

I have the STMf32f469 board , when I try to send a demo to the board it says that I do not have the St link utility ? Shouldnt I have got that with the StmCube install ? Or do I need to download that specifically ?

EDIT> Worked with ST link. Although it is just in one corner of the screen , resolution issue .

Although the demo should be set to 800x480 ? === I can only select the STM32f469I and not the STM32f469. Is my board not supported and is the I version higher resolution ?

Or are the demos made for smaller screens ?

Is there a get started PDf or something somewhere , there is way too much on the STm site and I get confused , can someone point me to a get started thingy ?

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0