2015-02-08 2:36 PM
Hello,
I'm using IAR EWARM 6.70.1.5794 for developping a firmware on a STM32F107VCT6. I use a ST LINK V2 for debug. Now i would like generate an hex or bin file for downloading the file without ST-LIN V2 but with Flash Loader Demonstrator in bootloader mode. I have tried Project -> Options -> Output Converter -> Generate additional output file / Intel extended but when i try to load the file with Flash Loader demonstrator, i have an error : ''unable to load this file...'' I have although tried to unselect ''include debug information in output'' but that's the same problem =( Anyone have an idea to solve this? Thanks #flash-demonstrator-iar-hex2015-02-08 5:40 PM
What address did you build the code for? 0x00000000 or 0x08000000
Could you attach the .HEX you've built currently? Would be useful to identify what the problem is.2015-02-08 10:58 PM
Apparently, the ROM start at 0x08000000.
/*-Memory Regions-*/ define symbol __ICFEDIT_region_ROM_start__ = 0x08000000; define symbol __ICFEDIT_region_ROM_end__ = 0x080FFFFF; define symbol __ICFEDIT_region_RAM_start__ = 0x20000000; define symbol __ICFEDIT_region_RAM_end__ = 0x20017FFF; /*-Sizes-*/ define symbol __ICFEDIT_size_cstack__ = 0x400; define symbol __ICFEDIT_size_heap__ = 0x200; ________________ Attachments : Project.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hz2o&d=%2Fa%2F0X0000000bMx%2FB3MiP8mo_LOdmsAPKs5c4xAgRHV60CANuA2JLPF1n_I&asPdf=false