2010-09-22 8:24 AM
FSMC acces mode
2011-05-17 5:08 AM
Hello,
Is there somebody to help me to understand FSMC configuration. Thank you in advance. Eric2011-05-17 5:08 AM
read this Application Note for complete understanding (AN2784)
http://www.st.com/stonline/products/literature/anp/14779.pdf
hope this will help.
2011-05-17 5:08 AM
Hello,
Thank you for your response. Yes, I see AN2784 application note. But for read timing, I can't see any difference between Figure 3 for Flash and Figure 6 for SRAM except for NADV signal which is don't care for non-multiplexed access. For write timing, I can't see any difference between Figure 4 for Flash and Figure 6 for SRAM. So I don't know the effect of choosing 10b (Flash) or 00b (Ram) for MTYP.When I display signal on a oscilloscope, it seems there is no change when I use 10b or 00b for MTYP.
Eric