cancel
Showing results for 
Search instead for 
Did you mean: 

FSMC 8 bit bus

noamashual
Associate
Posted on September 22, 2014 at 16:21

hey all,

i am using STM32F4 MCU. trying to connect LCD controller (ILI9342C) using FSMC.

i understand that i can use the 8 bit bus.

how can i determine which bus to use : D0-D7 or D8-D15

Thanx

#fsmc
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on September 22, 2014 at 17:35

On the STM32 side or the LCD Controller side.

From the STM32 D8..15 would only be present if you used at 16-bit bus, and shifted the data into the high order byte

The key difference in 16-bit mode is that the sense of A0, and other address bits, is shifted
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..