2025-09-22 4:28 AM
Sorry, I'm very new to microcontrollers in general and was wondering if I would need more SRAM or if I could successfully just write to the display driver's memory and not worry about a big frame buffer. I hope to use LVGL to control a 320x240 16 bit colour depth display using this method, any help on this topic would be greatly appreciated, thank you.
For reference, the reason I'm interested in doing this is because I'm using the STM32 F4VE Black board and I can see it has a TFT interface.
Solved! Go to Solution.
2025-09-22 4:46 AM - edited 2025-09-22 4:53 AM
Hello,
Yes you can use FSMC to drive ILI9341 display.
A video from Youtube.
You can also refer to the implementation and inspire from the ILI9341 driver on the STM324G_EVAL
You can also refer to the BSP example and use: https://github.com/STMicroelectronics/STM32CubeF4/blob/master/Projects/STM324xG_EVAL/Examples/BSP/Src/lcd.c
The FSMC intilization is provided in stm324xg_eval.c / LCD_IO_Init() that calls FSMC_BANK3_Init():
static void FSMC_BANK3_Init(void)
{
SRAM_HandleTypeDef hsram;
FSMC_NORSRAM_TimingTypeDef SRAM_Timing;
/*** Configure the SRAM Bank 3 ***/
/* Configure IPs */
hsram.Instance = FMC_NORSRAM_DEVICE;
hsram.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
SRAM_Timing.AddressSetupTime = 5;
SRAM_Timing.AddressHoldTime = 1;
SRAM_Timing.DataSetupTime = 9;
SRAM_Timing.BusTurnAroundDuration = 0;
SRAM_Timing.CLKDivision = 2;
SRAM_Timing.DataLatency = 2;
SRAM_Timing.AccessMode = FSMC_ACCESS_MODE_A;
hsram.Init.NSBank = FSMC_NORSRAM_BANK3;
hsram.Init.DataAddressMux = FSMC_DATA_ADDRESS_MUX_DISABLE;
hsram.Init.MemoryType = FSMC_MEMORY_TYPE_SRAM;
hsram.Init.MemoryDataWidth = FSMC_NORSRAM_MEM_BUS_WIDTH_16;
hsram.Init.BurstAccessMode = FSMC_BURST_ACCESS_MODE_DISABLE;
hsram.Init.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_LOW;
hsram.Init.WrapMode = FSMC_WRAP_MODE_DISABLE;
hsram.Init.WaitSignalActive = FSMC_WAIT_TIMING_BEFORE_WS;
hsram.Init.WriteOperation = FSMC_WRITE_OPERATION_ENABLE;
hsram.Init.WaitSignal = FSMC_WAIT_SIGNAL_DISABLE;
hsram.Init.ExtendedMode = FSMC_EXTENDED_MODE_DISABLE;
hsram.Init.AsynchronousWait = FSMC_ASYNCHRONOUS_WAIT_DISABLE;
hsram.Init.WriteBurst = FSMC_WRITE_BURST_DISABLE;
hsram.Init.PageSize = FSMC_PAGE_SIZE_NONE;
/* Initialize the SRAM controller */
FSMC_BANK3_MspInit();
HAL_SRAM_Init(&hsram, &SRAM_Timing, &SRAM_Timing);
}
You may need to change the FSMC timings if needed.
Hope that helps.
2025-09-22 4:46 AM - edited 2025-09-22 4:53 AM
Hello,
Yes you can use FSMC to drive ILI9341 display.
A video from Youtube.
You can also refer to the implementation and inspire from the ILI9341 driver on the STM324G_EVAL
You can also refer to the BSP example and use: https://github.com/STMicroelectronics/STM32CubeF4/blob/master/Projects/STM324xG_EVAL/Examples/BSP/Src/lcd.c
The FSMC intilization is provided in stm324xg_eval.c / LCD_IO_Init() that calls FSMC_BANK3_Init():
static void FSMC_BANK3_Init(void)
{
SRAM_HandleTypeDef hsram;
FSMC_NORSRAM_TimingTypeDef SRAM_Timing;
/*** Configure the SRAM Bank 3 ***/
/* Configure IPs */
hsram.Instance = FMC_NORSRAM_DEVICE;
hsram.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
SRAM_Timing.AddressSetupTime = 5;
SRAM_Timing.AddressHoldTime = 1;
SRAM_Timing.DataSetupTime = 9;
SRAM_Timing.BusTurnAroundDuration = 0;
SRAM_Timing.CLKDivision = 2;
SRAM_Timing.DataLatency = 2;
SRAM_Timing.AccessMode = FSMC_ACCESS_MODE_A;
hsram.Init.NSBank = FSMC_NORSRAM_BANK3;
hsram.Init.DataAddressMux = FSMC_DATA_ADDRESS_MUX_DISABLE;
hsram.Init.MemoryType = FSMC_MEMORY_TYPE_SRAM;
hsram.Init.MemoryDataWidth = FSMC_NORSRAM_MEM_BUS_WIDTH_16;
hsram.Init.BurstAccessMode = FSMC_BURST_ACCESS_MODE_DISABLE;
hsram.Init.WaitSignalPolarity = FSMC_WAIT_SIGNAL_POLARITY_LOW;
hsram.Init.WrapMode = FSMC_WRAP_MODE_DISABLE;
hsram.Init.WaitSignalActive = FSMC_WAIT_TIMING_BEFORE_WS;
hsram.Init.WriteOperation = FSMC_WRITE_OPERATION_ENABLE;
hsram.Init.WaitSignal = FSMC_WAIT_SIGNAL_DISABLE;
hsram.Init.ExtendedMode = FSMC_EXTENDED_MODE_DISABLE;
hsram.Init.AsynchronousWait = FSMC_ASYNCHRONOUS_WAIT_DISABLE;
hsram.Init.WriteBurst = FSMC_WRITE_BURST_DISABLE;
hsram.Init.PageSize = FSMC_PAGE_SIZE_NONE;
/* Initialize the SRAM controller */
FSMC_BANK3_MspInit();
HAL_SRAM_Init(&hsram, &SRAM_Timing, &SRAM_Timing);
}
You may need to change the FSMC timings if needed.
Hope that helps.