2014-01-22 7:25 AM
Hi all,
I use matlab to generate c code and have this code compile in IAR for STM32F4 as a library. So I have no ST libraries added just the c code and h files from matlab. Matlab uses sqrt, sin functions etc. declared at math.h, these functions use double and I'm looking for a way to force the compiler to use float (so the FPU will be used), I can't go through the entire code and switc every function used for the float equivalent. is there a simple way to do so? Thank you #math.h2014-01-23 6:54 AM
... freaking forum software ...