cancel
Showing results for 
Search instead for 
Did you mean: 

For STM32L552 with external SMPS (variant P). This variant has dedicated pins for VDD12 external power supply, but suppose I did not wish to use this SMPS, instead using the standard linear regulators. How do I connect the two VDD12 pins as unused?

MN.3
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

The datasheet indicates they're not connected when LDO is used, in which case you can leave them floating.

0693W00000KbCybQAF.png 

https://community.st.com/s/question/0D53W00000qwAkTSAU/external-smps-vdd12-pin-supply-required

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Guru

The datasheet indicates they're not connected when LDO is used, in which case you can leave them floating.

0693W00000KbCybQAF.png 

https://community.st.com/s/question/0D53W00000qwAkTSAU/external-smps-vdd12-pin-supply-required

If you feel a post has answered your question, please click "Accept as Solution".