Skip to main content
MFail.11
Associate III
June 3, 2021
Solved

External SMPS VDD12 pin supply required?

Hi,

I have to use STM32L562CEU6P on my project.

This uP has two VDD12 pin for external SMPS.

My question is simple, this SMPS supply is required or can I left this pins floating?

I don't need this feature and manual is not very clear.

Thanks in advance.

This topic has been closed for replies.
Imen GH
Imen GHBest answer
ST Employee
June 3, 2021

Hello @MFail.1​ ,

Welcome to STM32 Community!

Please refer to RM0438 (Section 8 Power control (PWR)) 

0693W00000BZz0LQAT.pngif an external SMPS is used, these pins must be connected.

otherwise (i.e. LDO is used for Vcore) these pins can be NC.

Imen

3 replies

Imen GH
Imen GHBest answer
ST Employee
June 3, 2021

Hello @MFail.1​ ,

Welcome to STM32 Community!

Please refer to RM0438 (Section 8 Power control (PWR)) 

0693W00000BZz0LQAT.pngif an external SMPS is used, these pins must be connected.

otherwise (i.e. LDO is used for Vcore) these pins can be NC.

Imen

MFail.11
MFail.11Author
Associate III
June 3, 2021

Thank you so much, I have not seen this note at my first look.

Imen GH
ST Employee
June 3, 2021

Please select my answer as Best if it fully answered your question, so that this thread will marked as solved.