FMC initialising and RTC desactivation
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-19 4:09 PM
Dear All,
I designed a HMI board with STM32F767 and QSPI NOR flash and MT48LC16M SDRAM with external OSC 8MHz and MC-306 32.768 KHz.
Approximately I tested more than 100 PCs of this board and all work without any problem.
but during this week in some new boards, I saw when I initialise FMC, the RTC does not work anymore. even with RTC again initialising, it still doesn’t work and need to get restarted or power off.
I also tested with internal LSI but nothing changes. I also connected V BAT to VDD the problem is still there.
funny thing that this software works in many of these boards, but some of them have exactly the same problem.
I also removed the SDRAM and NoR flash chips, but again had same problem.
Any body have had this problem?
- Labels:
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-02 2:08 AM
Hello,
Not obvious to tell what the problem is as there is no relation between FMC and RTC. You need to start a debug session and check where it fails in your code. Check all the return HAL APIs especially those of the RTC it may indicate the fail.