Skip to main content
geoffreymbrown
Associate III
May 10, 2011
Question

flow control uart1 -- odd behavior

  • May 10, 2011
  • 3 replies
  • 708 views
Posted on May 10, 2011 at 16:50

I'm trying to get flow control working on Uart1 on the discovery board and am seeing some odd behavior.  I have a little test program that receives 10 characters, pauses, and then echos them back.   At the host (linux) side I'm using a cp2102 based usb/uart bridge with the flow control pins brought out.  The cp2102 isn't consistently stopping when the stm32 raises RTS.  When it continues to send, the stm32 lowers (enables) RTS and leaves RTS enabled until the next time the stm32 firmware reads a character from the uart buffer.

Obviously the cp2102 issue is outside the scope of this forum, but I'm surprised that the response of the stm32 uart is to enable RTS.   I've attached a screenshot from the logic analyzer.  I'm curious if anybody understands what's going on with the stm32 end of things.

Here is my UART initialization and the key test loop:

int  uart_open (uint8_t uart, uint32_t baud, uint32_t flags)

{

  USART_InitTypeDef USART_InitStructure;

  GPIO_InitTypeDef GPIO_InitStructureTx;

  GPIO_InitTypeDef GPIO_InitStructureRx;

  if (uart == 1) {

    // Turn on clocks                                                                            

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA  |

                           RCC_APB2Periph_AFIO,

                           ENABLE);

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);

    // Configure TX pin                                                                          

    GPIO_InitStructureTx.GPIO_Pin = GPIO_Pin_9;

    GPIO_InitStructureTx.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_InitStructureTx.GPIO_Speed = GPIO_Speed_2MHz;

    GPIO_Init(GPIOA, &GPIO_InitStructureTx);

    // Configure RX pin                                                                          

    GPIO_InitStructureRx.GPIO_Pin = GPIO_Pin_10;

    GPIO_InitStructureRx.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_InitStructureRx.GPIO_Speed = GPIO_Speed_2MHz;

    GPIO_Init(GPIOA, &GPIO_InitStructureRx);

    // Configure CTS pin                                                                         

    GPIO_InitStructureRx.GPIO_Pin = GPIO_Pin_11;

    GPIO_InitStructureRx.GPIO_Mode = GPIO_Mode_IN_FLOATING;

    GPIO_InitStructureRx.GPIO_Speed = GPIO_Speed_2MHz;

    GPIO_Init(GPIOA, &GPIO_InitStructureRx);

    // Configure RTS pin                                                                         

    GPIO_InitStructureTx.GPIO_Pin = GPIO_Pin_12;

    GPIO_InitStructureTx.GPIO_Mode = GPIO_Mode_AF_PP;

    GPIO_InitStructureTx.GPIO_Speed = GPIO_Speed_2MHz;

    GPIO_Init(GPIOA, &GPIO_InitStructureTx);

    // Configure the UART                                                                        

    USART_StructInit(&USART_InitStructure);

    USART_InitStructure.USART_BaudRate = baud;

    USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_RTS_CTS;

    USART_Init(USART1,&USART_InitStructure);

    USART_Cmd(USART1, ENABLE);

    return 0;

  }

}

ssize_t uart_write(uint8_t uart, const void *buf, size_t nbyte)

{

  int i;

  for (i = 0; i < nbyte; i++)

    {

      while (!(USART1->SR & USART_FLAG_TXE));

      USART1->DR =  ((uint8_t *) buf)[i];

    }

}

ssize_t uart_read (uint8_t uart, void *buf, size_t nbyte)

{

  int i;

  for (i = 0; i < nbyte; i++)

    {

      while (!(USART1->SR & USART_FLAG_RXNE));

      ((uint8_t *) buf)[i] =  USART1->DR & 0xff;

    }

  return i;

}

 while(1)

  {

    Delay(20);

    uart_read(1, buf, 10);

    Delay(20);

    uart_write(1,buf,10);

  }

#uart-flow-control #cts #rts
This topic has been closed for replies.

3 replies

geoffreymbrown
Associate III
May 10, 2011
Posted on May 10, 2011 at 21:10

I found a partial answer to my question. The cp2102 (and similarly the ftdi parts) continues to send 1 to several bytes after its CTS line goes high (RTS from the stm32).

Thus, the only way to reliably use it is to keep a software receive buffer and raise RTS with software (at the stm32) when the buffer is nearly full.  I guess this begs the question -- what use is hardware controlled RTS on the stm32 if there is only a single character buffer ?

Andrew Neil
Super User
May 16, 2011
Posted on May 16, 2011 at 08:25

''The cp2102 (and similarly the ftdi parts) continues to send 1 to several bytes after its CTS line goes high (RTS from the stm32)''

 

 

Yes, it is ''normal behaviour'' for any device to continue to send ''a few'' characters after flow control is asserted.

''I guess this begs the question -- what use is hardware controlled RTS on the stm32 if there is only a single character buffer?''

Yes, that is a very good question!

/4108fad7

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
sundar
Associate III
March 5, 2014
Posted on March 05, 2014 at 09:01

How to Assert or de assert RTS/CTS