Question
STM32F405RG SWDIO, SWCLK, SWO, NRST pin connections
Posted on March 04, 2014 at 12:59
Hi ,
I am about to draw the schematics of a card which has STM32F405RG on it. I want to program my card throug SWD port. I made the pin connections as I described below: NRST: pulled up to VDD with 100K SWDIO: pulled up to VDD with 100K SWCLK : pulled down to GND with 100K. Are these conections are correct? I have STM32F4 discovery kit when I look at the schematics of the discovery board I see that SWDIO is pulled to low, SWCLK is p?lled to high and NRST is pulled to high. However on the documenthttp://support.code-red-tech.com/CodeRedWiki/HardwareDebugConnections
it is recommended to connect as I did.I could not decide which one is correct. I will be very glad if you can help me. Thank you very much. .. tugba #jtag