cancel
Showing results for 
Search instead for 
Did you mean: 

Flashing STM32 with hyper terminal using inbuilt bootloader

rsh.1
Associate II

Hi,
I was flashing the STM32 Nulceo_h723zg which is having inbuilt primary bootloader in STMCube programmer, by making BOOT pin high via UART.

But i want to flash by using hyper terminals like teraterm.

How can we send binary or hex files into stm board by using such terminal.

Thanks.

10 REPLIES 10

>STMProgrammer have this code inbuild, why dont use ???

Yeah. Should be possible to add a teraterm menu command or "macro" that runs STM32_Programmer_cli with a cooked command line ...