2023-06-28 9:25 AM - last edited on 2023-06-30 9:15 AM by STOne-32
Hi,
I was flashing the STM32 Nulceo_h723zg which is having inbuilt primary bootloader in STMCube programmer, by making BOOT pin high via UART.
But i want to flash by using hyper terminals like teraterm.
How can we send binary or hex files into stm board by using such terminal.
Thanks.
2023-07-02 3:37 AM
>STMProgrammer have this code inbuild, why dont use ???
Yeah. Should be possible to add a teraterm menu command or "macro" that runs STM32_Programmer_cli with a cooked command line ...