2017-02-05 4:11 AM
Hello I am new with using the BlueNRG1, so I am having trouble flashing the STEVAL-IDB007V1. I'm trying to get the binary image to upload it to the BlueNRG and I'm using ATOLLIC TrueSTUDIO to compile my version of hello word. I have looked everywhere in ATOLLIC TrueSTUDIO and cannot find where to download the the binary image file so that I could then use the BlueNRG GUI to flash the BlueNRG. Is this the correct way to go about this or am I going to have to get the ST-Link to flash it directly?
I'm using
ATOLLIC TrueSTUDIO v7.1.0
#flash-uc #get-started2017-02-06 1:58 AM
Hello Marco
I have moved your question to the
‌ where someone should be able to assist you.Thanks
Oli
2017-02-15 10:37 AM
Hello Marco Carmona,
Maybe you can try
following the User manual for BlueNRG-1 ST-LINK Utility software description.Regards
Imen