cancel
Showing results for 
Search instead for 
Did you mean: 

Flash read through debugger not working when using WFE/WFI

Arlet Ottens
Associate II

I am using an STM32F429VGT6 with SWD debugger, and OpenOCD software 0.10.0.

I am trying to dump the contents of the flash memory at 0x08000000.

If I don't use any WFE/WFI in my code, this works fine.

If I put a WFE at the beginning of the code, before any interrupts are enabled, the device is in continuous SLEEP mode, and I also have no problems reading the flash memory.

However, when I used WFE in normal code, and the device is switching between run/sleep modes, I sometimes get the wrong output when dumping the flash. There are no errors reported, but it just shows the wrong data.

In all cases, the debugger sets DBGMCU_CR to 7. I am not using STOP/STANDBY mode, just sleep.

I have also tried this on a STM32F427VIT6, and everything works fine there.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0