cancel
Showing results for 
Search instead for 
Did you mean: 

Flash - Ram

florianaugustin9
Associate II
Posted on August 21, 2012 at 20:28

Oh, thats a really nice idea. I'm running 168 Mhz so i have 5 wait states for the flash.

But unfortunately i have no idea if i'm running from flash or ram.

I used the standard settings from Crossworks IDE. If I compile the project there are 4.8 kb of flash used and 0.2 kb ram. I suppose it runs from flash? 

And I would be really glad if you could explain the pipeline thing to me. I basically know what pipeline is from university, but i did'nt get it.

Thank you for your help!
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0