2018-05-28 11:44 PM
Hi all, am getting error from flash load demonstrator v2.8 when connecting STM32nucleoF401RE and X NUCLEO WIFI IDWO1M1 , when upgrading UART firmware 'unrecognized device .. please reset your device and try again' or ' No response from target bootloader cannot started please verify bootmode configuration and the flash protection status.. rest your device and try again'
2018-05-29 12:37 AM
Hello,
What is the number of detected VCOM of your Nucleo board?
Please try to clean not used virtual COM ports to have this number <100.
Best Regards,
Artur
2018-05-30 5:10 AM
COM4 is the virtual COM port number.. am using windows 10 in my pc.. don't know whether windows and flash loader demo version matching is the problem .
2018-05-30 5:53 AM
Hello
remyaramaswamy1991
,Try to use t
he
http://www.st.com/en/development-tools/stm32cubeprog.html?icmp=tt6237_gl_****_dec2017
softwaretool
offer in one place all services, which were provided by existing tools (
ST Visual Programmer, DFUse Device Firmware Update tool, Flash Loader, and ST-Link utility
).
With Regards,
Imen
2018-05-31 12:50 AM
hi thank you. how to set boot mode in X Nucleo IDW01M1 board while upgrading UART firmware