cancel
Showing results for 
Search instead for 
Did you mean: 

Flash error when programming STM32F407

mcwilliams
Associate
Posted on May 29, 2013 at 16:34

Hi, I have an STM32F407IE on a custom board and I am programming/debugging with an Olimex ARM-USB-TINY-H using OpenOCD.  I have come across this error with two separate microcontrollers now.  It seems as though the microcontroller enter some type of error state while running (I have not had it attached to the debugger when this error happens).  Once it occurs, I try running it through the debugger and it refuses to run.  When running it through gdb, it gives me the following:

stm32f4x.cpu -- clearing lockup after double fault

Program received signal SIGINT, Interrupt.

Using OpenOCD, I can issue a 'reset halt' command to halt the microcontroller, but when I do a 'flash probe 0', I get the following response:

device id = 0x10016413

JTAG-DP STICKY ERROR

MEM_AP_CSW 0x23000051, MEM_AP_TAR 0x1fff7a24

STM32 flash size failed, probe inaccurate - assuming 1024k flash

flash size = 1024kbytes

flash 'stm32f2x' found at 0x08000000

If I try to erase the flash and write a new image, I get the following error:

auto erase enabled

stm32x device protected

failed erasing sectors 0 to 7

in procedure 'flash'

I know all of this is specific to OpenOCD, but it seems like this is a hardware issue.  It seems like occasionally something is happening to the flash.  I am not using any flash-specific calls in code from the stm32f4xx_flash.h library.  Does anyone have any suggestions?  Any other logging information that I could provide to help?

#solution-stm32f407-flash-openocd #jtag #flash-openocd-jtag-sticky-error #jtag-olimex
This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Posted on May 29, 2013 at 16:49

All the open stuff is rather half-assed, you do however have the source if you want to dig in. You could perhaps address this with the devs in an OpenOCD forum, but I suspect the response will be disappointing.

The errors are somewhat indicative of a JTAG/SWD communication issue, perhaps also power, clocks, or resets.

You might want to try something designed with more rigor, like a Segger J-Link, and see if it spits out any more useful diagnostics, or recovers in a more elegant fashion. As this is a custom board, your biggest hurdle will be to validate your own hardware, and understand what it's doing, and why.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
johnjohn9106
Associate
Posted on May 30, 2013 at 07:28

Something caught my eye:

   ''stm32x device protected''

 

Could this be the cause of your troubles?

The inexpensive ST-LINK/V2 has a nice GUI that can quickly unlock the flash.  Ref https://my.st.com/st-extranet-web-active/active/en/catalog/tools/PF251168

Sometimes available from Digikey:

http://www.digikey.com.au/product-search/en/programmers-development-systems/in-circuit-programmers-emulators-and-debuggers/2621880?k=st-link
emalund
Associate III
Posted on May 30, 2013 at 16:53

custom board ...  [most boards work, but] I have come across this error with two separate microcontrollers now

 

if my edit above is correct, this would be a typical result of a missing pullup/pulldown resistors
jpeacock2399
Associate II
Posted on May 30, 2013 at 21:39

In my experience JTAG resistors aren't needed on F2 and F4 parts; the internal pullups/pulldowns seem to work fine unless the GPIO settings are altered.  I have a custom board with an STM32F205 that works fine (using Segger J-Link) without resistors.

I seem to recall there was some errata on F1 parts about the internal resistors though.

  Jack Peacock
jpeacock2399
Associate II
Posted on May 30, 2013 at 21:48

stm32f4x.cpu -- clearing lockup after double fault

This means your program is generating a hard fault, usually a double fault condition (fault within the fault handler).  Do you intercept any of the fault interrupts?  It makes debugging a whole lot easier if you do.

device id = 0x10016413

This is a Rev Z (0x1001), STM32F407 (0x413), so you are correctly reading the MCU device code.  Since the Olimex doesn't recognize it my guess is your JTAG software doesn't include definitions for the STM32F4 series.

Jack Peacock
billr1
Associate II
Posted on May 31, 2013 at 05:43

Recent versions of the OpenOCD software do support the STM32F4xx series. There is a specific target config file for that CPU. Make sure you have it specified in your board config file. For example, I'm using an Olimex H407 demo board with the same JTAG adapter you are and my board file looks like this:

source [find interface/olimex-arm-usb-tiny-h.cfg]

source [find target/stm32f4x.cfg]

I also have a programming issue with the F407, but it's not the same as yours. I am able to erase and program the first time after OpenOCD is started, but the next time through on the same session results in a programming error:

Error: timeout waiting for algorithm, a target reset is recommended

Error: error executing stm32x flash write algorithm

Error: flash write failed = 00000040

Error: error writing to flash at address 0x08000000 at offset 0x00000000

in procedure 'flash'

Error: stm32f4x.cpu -- clearing lockup after double fault

The way around this is to kill the OpenOCD server and restart it. I strongly suspect this is an OpenOCD error, because it was working ok on earlier versions of OpenOCD.
pacman
Associate III
Posted on January 13, 2015 at 12:19

I had the exact same issue. The fix is in

/ee76e9e1

.