2021-07-30 2:24 AM
Hi,
I'am reading data through USART1 and USART2. I am sending the data over USART3 using printf. It works for a while but then stops.
Here is my code:
FILE *stream;
char *buf;
size_t len;
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
if (huart->Instance == USART1)
{
uart_1_Ready = SET;
HAL_UART_Receive_IT (&huart1, UART_1_rxBuffer, UART_1_RX_BUFFER_SIZE);
fprintf(stream, UART_1_rxBuffer);
}
else if (huart->Instance == USART2)
{
uart_2_Ready = SET;
HAL_UART_Receive_IT (&huart2, UART_2_rxBuffer, UART_2_RX_BUFFER_SIZE);
fprintf(stream, UART_2_rxBuffer);
}
}
void sendDataUsart3(void)
{
if(len >= 600)
{
printf(buf);
fclose(stream);
free(buf);
buf = (char *)realloc(buf, 600);
stream = open_memstream(&buf, &len);
}
}
int main(void)
{
buf = (char *) malloc(600);
stream = open_memstream(&buf , &len);
....
}
2021-07-30 6:50 AM
Hello asttekin,
Correct me if I'm wrong, but I don't think you should free(buf) before realloc(buff...). realloc is expecting a valid pointer to allocated memory(?)
Regards,
Dave
2021-07-30 9:05 AM
How do you ensure the buffers are properly NUL terminated?
Any code to recover the situation if the receiver overruns or gets some framing or parity error?
2021-07-30 10:37 AM
Actually I don't know exactly how to do it.I am using FILE stream for the first time in a project.
I manually insert the NULL after each UART data read.The UART data receiving code is as follows.Same as USART2.
if (huart->Instance == USART1)
{
uart_1_Ready = SET;
uart_1_Timeout = 0;
HAL_UART_Receive_IT (&huart1, UART_1_rxBuffer, UART_1_RX_BUFFER_SIZE);
tempUart_1_Val = huart->Instance->DR;
if (tempUart_1_Val == '$')
{
uart_1_record = 1;
nmea_1_InputBufferIndex = 0;
}
if (uart_1_record)
{
nmea_1_InputBuffer[nmea_1_InputBufferIndex] = tempUart_1_Val;
nmea_1_InputBufferIndex++;
if (tempUart_1_Val == 0x0A)
{
nmea_1_InputBuffer[nmea_1_InputBufferIndex] = '\0';
navDataInput_1_ChecksumHigh = nmea_1_InputBuffer[nmea_1_InputBufferIndex - 4];
navDataInput_1_ChecksumLow = nmea_1_InputBuffer[nmea_1_InputBufferIndex - 3];
uart_1_dataReceived = 1;
if(workingMode == MODE1)
{
nmea_1_InputBufferIndex = 0;
}
if (workingMode == MODE2)
{
fprintf(stream, nmea_1_InputBuffer);
memset(nmea_1_InputBuffer,'\0', NMEA_BUFFER_SIZE);
}
uart_1_record = 0;
}
}
}