cancel
Showing results for 
Search instead for 
Did you mean: 

field gpio_type could not be resolved error

jlchoobs
Associate II
Posted on May 28, 2012 at 18:51

Why should the App.h file with :

  /// PORTA[0..15] = Available :

  RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOA ,

ENABLE

); 

  GPIO_InitStructure.

GPIO_Pin

= (GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15 );

  GPIO_InitStructure.

GPIO_OType

=

GPIO_OType_OD

;

// OUT

 

GPIO_InitStructure.

GPIO_PuPd

=

GPIO_PuPd_UP

;

  GPIO_InitStructure.

GPIO_Speed

=

GPIO_Speed_100MHz

;

// GPIO_Speed_2MHz

 

GPIO_Init(GPIOA, &GPIO_InitStructure);

  GPIOA->

ODR

= (0xFFFFFFFF);

be Red-Marked as an error in Eclipse / Code Sourcery :

  field gpio_pin  could not be resolved

  field gpio_otype  could not be resolved

  field gpio_pupd  could not be resolved

  field gpio_speed  could not be resolved

- ?

The App.h includes stm32f4xx_gpio.h ,

and the stm32f4xx_gpio.h file does not show any errors.

This compiled in Atollic.

#code-sourcery-bug
1 REPLY 1
jlchoobs
Associate II
Posted on May 30, 2012 at 05:59

Resolved.

- missing USR_cb struct.