Skip to main content
Senior
September 5, 2024
Solved

Error Occurs When IMG Data is Moved to NOR Flash in Linker

  • September 5, 2024
  • 5 replies
  • 2567 views

I encountered an issue where an error occurs when only the image data is moved to NOR Flash in the linker. I have already verified that the NOR Flash works correctly in a separate project by toggling the LEDs.

In my current TouchGFX project, I enabled the NOR Flash in the IDE, and I am able to read the data in the memory browser, confirming that the same data is present.

However, when I choose my custom loader in the debug configuration and try to debug, 

 

If I remove the ext_flash section from the linker, I am able to debug and see the data in the memory browser.but its just txbuffer data(0xD20F- increases) My question is, if this error is resolved, will I be able to see the image data in the memory browser? This would help me confirm that the NOR Flash is indeed storing the image data correctly.

 

Any insights on why this might be happening or suggestions for resolving this issue?I get the following error:

Screenshot (1383).png

 

 

 

 

 ExtFlashSection :
 {
 . = ALIGN(4);
 *(.ExtFlashSection) 
 *(.ext_flash*) 
 KEEP(*(.image*)) 
 KEEP(*(.img*)) 
 KEEP(*(.assets*)) 
 . = ALIGN(4);
 } >EXT_FLASH

 

 

 

 

 

This topic has been closed for replies.
Best answer by jr_engr_mbed

here, is update --> i got able to enable norflash and load imgs., what i did is replaces actual flash which is 128mbits which is come along with eval-brd.. so, there is no data mismatch error occur.. so, this error is solved.. thank you.

5 replies

mƎALLEm
ST Technical Moderator
September 5, 2024

@jr_engr_mbed wrote:

will I be able to see the image data in the memory browser? This would help me confirm that the NOR Flash is indeed storing the image data correctly.

 


You said that the content of the Flash is OK. How are you sure? are you using CubeProgrammer? if yes, did you check the content when reading the Flash NOR, then compare it to what was shown in the CubeIDE debugger?

Also, did you add your loader in the CubeIDE in Debugger menu?

Example:

SofLit_0-1725547347887.pngSofLit_1-1725547443529.png

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Senior
September 5, 2024

"Yes, I am using the loader with CubeProgrammer and CubeIDE. As you asked me to check if the same data occurs, I will show you what I receive in both cases.

This is working in a separate NOR flash program without TouchGFX, as I can see the correct output."

Screenshot (1401).png

Screenshot (1405).png

 

“With TouchGFX, I can see the same output in both runs. However, when I debug multiple times, I occasionally get some 0xFFFF data in between. Could this indicate that my loader is not working correctly, assuming the NOR flash was the only memory enabled in the first program run?”

if img present in norflash which manually puts 

LOCATION_PRAGMA("ExtFlashSection")

KEEP extern const unsigned char image_alternate_theme_images_widgets_imageprogress_styled_batteries_battery_large[] LOCATION_ATTRIBUTE("ExtFlashSection") = { // 110x40 RGB565 pixels.

0x00, 0x00, 0x00, 0x00, 0x92.....)... i gets error?

Senior
September 5, 2024

as this is shows, with just touchgfx enabled..

Screenshot (1413).png

Screenshot (1411).png

jr_engr_mbedAuthorBest answer
Senior
October 21, 2024

here, is update --> i got able to enable norflash and load imgs., what i did is replaces actual flash which is 128mbits which is come along with eval-brd.. so, there is no data mismatch error occur.. so, this error is solved.. thank you.