cancel
Showing results for 
Search instead for 
Did you mean: 

How to Implement CANopen FD on STM32H753VIT6 (Already Using CAN FD)

pavanl
Associate II

Hello ST Community,

I am working on a project using the STM32H753VIT6 and have already successfully implemented CAN FD communication using the FDCAN peripheral and HAL drivers.

Now, I would like to implement CANopen FD on this setup.

My questions:

  1. What libraries or open-source stacks are available for CANopen FD that can be integrated with STM32 (CMSIS/HAL based)?

  2. What are the hardware or timing considerations for running CANopen FD at higher bitrates? My transceivers are currently non-isolated.

  3. How should I structure the implementation of:

    • Object Dictionary (OD)

    • USDO (Universal Service Data Object)

    • PDO (Process Data Object)

  4. Is there a reference example or demo project for CANopen FD (not classic CANopen) with STM32?

Any guidance, sample code, or links to documentation would be greatly appreciated.

Thanks in advance!


Pavan

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

To my knowledge there is no CANOpen open source for CAN-FD. While you can find an open source with CAN2.0.

Our partner Emotas offers CANopen FD stack on STM32G4. You can contact them over this link or over this email: ged@emotas.de (Torsten Gedenk).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
MHoll.2
Senior III

 

Hi,
I don't know any open source CANOpen FD stack (the most used CANopenNode Stack can be made CANOpen FD, but needs a lot of work, for example there is no USDO implementation).
There are some commercial stack claiming CANOpen FD functionalities (Emotas, MicroControl and others).

Oleksii
Senior

A common mistake when people try to implement a full-fledged CANopen interface on microcontrollers.
You should decide what your device does and implement hard logic with the services you really need.
Often in practice, these are a few device parameters, the rest is superfluous.

Oleksii
Senior
 
mƎALLEm
ST Employee

Hello,

To my knowledge there is no CANOpen open source for CAN-FD. While you can find an open source with CAN2.0.

Our partner Emotas offers CANopen FD stack on STM32G4. You can contact them over this link or over this email: ged@emotas.de (Torsten Gedenk).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
pavanl
Associate II

Thank you all for your responses. I appreciate the insights and information shared regarding CANopen support for CAN-FD. This helps me better understand the available options.