cancel
Showing results for 
Search instead for 
Did you mean: 

FD CAN doesn't work properly

MKami.0
Associate

What is the best way to set up FD CAN in classic mode on stm32 nucleo h743zi board?

Currently, I'm using FDCAN with 16 Mhz frequency on the bus and I want to get 500kbit/s.

My settings are:

hfdcan1.Init.NominalPrescaler=2;

hfdcan1.Init.NominalSyncJumpWidth=1;

hfdcan1.Init.NominalTimeSeg1=13;

hfdcan1.Init.NominalTimeSeg2=2;

hfdcan1.Init.DataPrescaler=1

hfdcan1.Init.DataSyncJumpWidth=2;

hfdcan1.Init.DataTimeSeg1=13;

hfdcan1.Init.DataTimeSeg2=2;

Using osciloscope I see that one bit is sending in 13 ms time, when it should be in 2 us.

How to set things up properly?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee

Hello,

I recommend you to follow the FDCAN example within STM32CubeH7, shows how to configure the FDCAN peripheral to send and receive

Classic CAN frames in normal mode:

STM32Cube_FW_H7_V1.3.2\Projects\STM32H743I_EVAL\Examples\FDCAN\FDCAN_Classic_Frame_Networking

Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen