2010-10-16 11:42 PM
hi.
i have aquestion: if i want the measure sevrel channels in the fastest way what are my options and how? thanks.2010-10-18 01:29 AM
2010-10-18 01:47 AM
> why does no one answers?
Maybe because there's very few people reading this forum? Maybe because the answer depends on what you are going to do with the samples, and when? And if your program need to do other things during the AD-conversion? And probably a couple of other things as well. Why don't you try some ways to do it, and tell us which is the fastest :)2010-10-18 02:19 AM
thanks for the replay it was not
complaint i simply didnt understand why.
what i meant was there are servel modes to work with the ADC scan mode single mode and so on. my question is which is better to use if you want to measure sevrel channels. thanks.