Posted on October 22, 2010 at 10:36From ''RM0041 Reference Manual'' for stm32f100xx, last paragraph in section 2.1:After each device reset, all peripheral clocks are disabled (except for the SRAM and FLITF). Before using a peripheral you have to en...
Posted on October 18, 2010 at 15:35You're welcome! By the way. I knew I've read the ld/md-definition somewhere. Now I found it. In the begining of every chapter in the reference manual it saysLow-density value line devices are STM32F100xx microcontr...
Posted on October 18, 2010 at 12:10You're supposed to use only one startup file. Which one depends on the device, cl - connectivity line ld - low density md - medium density hd - high density vl - value line So what is the stm32F100RBT6B? According ...
Posted on October 18, 2010 at 10:47> why does no one answers? Maybe because there's very few people reading this forum? Maybe because the answer depends on what you are going to do with the samples, and when? And if your program need to do other thi...
Posted on October 18, 2010 at 10:03> can you tell me what sould i correct in the pll please thanks. If you use the startup-files you don't have to do it yourself. Otherwise you can do as you do now (as I told you in another thread). But that solutio...